Added to cart
Added to cart
Go to shopping cart

COULD YOU IMAGINE THIS BEING REPAIRED IN 1 DAY?

Here’s what makes the Hilti tool service special.

WHAT MAKES THE HILTI TOOL SERVICE SPECIAL.

Hi, my name’s Om and I’m the new Services Product Manager for the Hilti Northern Europe Region. As I’m new to my role, in my first blog, I want to share with you something that pleasantly surprised me about Hilti Tool Service.

Picture your car. Although most of us take care to have our vehicles insured, there’s always that unfortunate fact that accidents and breakdowns happen. The worst of it is, it usually happens after the warranty period ends so you can end up paying large sums of money to repair it.

Fortunately, that’s not the case for Hilti tools. Hilti offer free repairs up to a 2-year repair warranty period commonly known as ‘no cost period’ where they’ll collect, repair and return the tools usually within 3 days.

Sounds good so far. But I bet you’re asking yourself, what happens when the 2 years ‘no-cost’ period comes to an end? Well, Hilti have thought of that too.

Once the tool is out of warranty Hilti offer the ‘3 days or free’ service which is a 3-day turnaround promise for chargeable repairs - if we fail to deliver on time, the repair charges are waived.

So, what is this ‘3 days or free’ service?

Hilti guarantees a 3-days repair service or the repair cost is borne by the company.

As the name suggests, if your tool breaks down, Hilti guarantees a 3-days repair service or the repair cost is borne by the company. In fact, the tool is fixed in just 1 day and the other 2 days are for the pick-up and drop-off. Sounds easy? Well, in this period – the repair call is scheduled, tool is picked up, tool is delivered to the repair centre, tool is opened for analysis, parts are replaced or repaired, the tool is assembled, tested, re-tested, cleaned, packaged, sent out for delivery and many more similar functions… still easy? Perhaps not. But at Hilti we believe in pushing the boundaries of what is possible – which is why we believe that no other competitor could ever match the 3 days or free promise.

Why is this service so special?

Hilti takes all this stress away because we all know that time is money and that matters to all of us!

After all, a tool breakdown could be stressful. Firstly, you are already frustrated because the breakdown will lead to operational downtime and delays in your project timeline. Secondly, you need to find out the details of the tools to schedule a repair. Finally, you need to spend money not only to repair the tool but also to ship it to the manufacturer’s service centre. Hilti takes all this stress away because we all know that time is money and that matters to all of us!

What are the advantages of this service?

We are constantly looking for more time and we know how precious time could be. Time does not wait and Hilti is never late, well almost!

There are several advantages that improve productivity and profitability. To make it easier I have broken this down by time and cost.

Time: We are constantly looking for more time and we know how precious time could be. Time does not wait and Hilti is never late, well almost! Read on….

  • Maximum downtime of 3 days: Tools are one of the most important resources on a jobsite and if it’s a matter of only 3 days – there are plenty of other jobs that workers can focus on. 3 days too long? Hilti has a service where you get a free loan tool so you don’t even need to wait the 3 days to crack on with job in hand!
  • Pick-up and drop-off: Don’t worry about having to drive around picking-up and dropping-off the tool, just call Hilti to report a repair and they take care of the logistics as well as the costs. When you call Hilti, they answer the call in 9 seconds (on average) and you’ll have the pleasure of chatting with a person and not a robot at the other end.
  • Don’t go hunting for your Purchase Order details: Usually when a tool breaks down we need to search our emails for the purchase order for a reference number but in the case of Hilti tools, the tool’s serial number is enough information to report a repair. Also, you don’t need to register a tool to be entitled to the warranty.
  • No repair quotation: To generate a repair quotation could take many days since the tool needs to be dismantled and analysed. But in the case of Hilti, they have a maximum cap on the repair cost so it can be sent to the repair centre without worrying about how much it would cost you.
Please enter alternative text here (optional)

Costs: There are many services that are not directly visible but they contribute significantly to your profitability. Look at how Hilti Tool Service plays an important role to your bottom line numbers.

  • Manufacturing defect: It is very rare for Hilti tools to have a manufacturing defect but if it happens – Hilti has a lifetime warranty for manufacturing defects.
  • No Cost Period’ Repair Warranty: This warranty is up to two years and is the best in class as it includes the wear and tear of the tools, batteries and chargers. This period can be extended up to 5 years.
  • Repair cost limit: Once the repair warranty is over, Hilti guarantees a cost limit for all future repairs which is equivalent to 40% of the price of a new tool, eliminating the high repair costs concern.
  • Repair quality: Wouldn’t you have sleepless nights if you had recently paid for a tool repair and it breaks down again? If you have recently paid for a repair and the tool breaks down within 3-months after this repair, Hilti offers the next repair for free.

With all that Hilti offers, I hope you’ll also be pleasantly surprised too at the service that comes as standard on Hilti tools.

At Hilti, we care about the success of your business. Minimising the time wasted and the costs to repair tools over their lifetime are perceived as the two most important factors in tool aftersales services. Although I’m new to my role, I’m confident Hilti delivers a best in class service offering - in more than 95% of the cases the tools are repaired within the 3-days period. On the odd occasion that we don’t manage it, at least you know your repair will be free!
 

CONTACT US
CONTACT US