Update of quantity
Please note, the order volume has been updated. This is due to package and minimum order quantities.
Please note, the order volume has been updated to. This is due to package and minimum order quantities.
Krøyers Plads is an exciting new build in the heart of Copenhagen’s old city with a history dating back to 1747.
It’s a challenging build because of its location and historical importance. And it’s also an important build, as it’s the first to be built under Denmark’s stringent new codes for green building, the so-called Nordic Swan or Svanemaerket codes.
The project is a mix of 20,000 m2 of offices, retail and housing. All of it needs to live up to Danish BR 15 energy regulations and will be visually green, with one façade and the roof covered with vegetation.
This was a big green building challenge, but we were more than able to help with one of our Clean-Tec products, designed to exceed statutory environmental requirements.
So while our Hilti engineers gave advice and technical calculations, our Hilti HIT-CT1 Clean-Tec adhesive was just right for post-installation rebars, matching the Nordic Swan codes, with a mal code of 00-3.
QUICK LINKS
To see account specific prices and content, please choose appropriate account.