5. Usage Restrictions
When using the Services, the Customer must fully comply with the following Usage Restrictions and is solely responsible to implement the required mitigation steps using its best efforts to avoid any potential incorrect usage:
Any and all Assets shall be handled according to the principles, formulas and security regulations and in accordance with the manufacturer`s technical directions and operating, mounting and assembly instructions, etc., that must be strictly complied with. Any Assets shown in the Software are based on the data Customer puts in. Therefore, Customer bears the sole responsibility for the absence of errors, the completeness and the relevance of the data to be put in by Customer. Further, the data captured in the Software may not represent all data needed to assess the health / monitoring of an Asset. Therefore, Customer bears sole responsibility for monitoring the Asset`s (i) maintenance schedule, (ii) lifecycle management, and (iii) physical Asset inspection from time to time. The Software only serves as a monitoring assistance, but without any warranty or guarantee as to the absence of errors, the correctness or fitness for any intended purpose. Customer must take all necessary and reasonable steps to prevent or mitigate damage caused by the usage of the Services. For complex and sensitive Assets, the involvement of a professional expert for inspecting and maintaining the Assets according to the Asset`s applicable operational menu needs to be adhered to by the Customer and is highly recommend by the Service Provider. Hilti will not be responsible in any means for restoring tenant based data.
Hilti is responsible in any means for neither the API integrations built by 3rd parties or by customers nor for the functionalities of the 3rd party application pre-integrated with ON!Track. Hilti is not responsible in any means for data loss, corruption, and edit in relation with an integration. The ON!Track Unite API credentials shall be kept in a secure place and not shared with 3rd parties. The ON!Track Unite API are offered for ordinary data integration, and not for any purpose of data mining, high load calls, abusive calls or for other data gathering purposes.
The functionalities offered during the current ON!Track Unite beta-phase shall be used for evaluation purposes and may not comply with legal and/or regulatory requirements. Hilti will have no liability for any harm or damage arising out of or in connection with the beta-functions, with the discontinuation of the Beta-Functions (Hilti may decide, to its sole discretion, to discontinue the beta-functionalities or selected APIs).