PD-E
 English
Information about the operating instructions
About these operating instructions
- Read these operating instructions before the product is used or operated for the first time. This is a prerequisite for safe, trouble-free handling and use of the product.
- Observe the safety instructions and warnings in these operating instructions and on the product.
- Always keep the operating instructions with the product and make sure that the product is accompanied by these operating instructions only, when the product is given to other persons.
Explanation of symbols
Warnings
Warnings alert persons to hazards that occur when handling or using the product. The following signal words are used:Symbols in the operating instructions
The following symbols are used in these operating instructions:|  | Comply with the operating instructions | 
|  | Instructions for use and other useful information | 
|  | Dealing with recyclable materials | 
|  | Do not dispose of electric equipment and batteries as household waste | 
Symbols in illustrations
The following symbols are used in illustrations:|  | These numbers refer to the illustrations at the beginning of these operating instructions. | 
|  | The numbers in illustrations refer to important work steps or to components important for the work steps. In the text, the corresponding numbers draw attention to these work steps or components, e.g. (3) . | 
|  | Item reference numbers are used in the overview illustration and refer to the numbers used in the key in the product overview section. | 
|  | This symbol is intended to draw your special attention to certain points for handling the product. | 
Product-dependent symbols
General symbols
Symbols used in relation to the product.|  | KCC‑REM-HLT‑PD-E | 
|  | On/off button | 
|  | Measure button | 
|  | Menu button | 
|  | Delete (clear) button | 
|  | Right arrow button | 
|  | Left arrow button | 
Product information
 products are designed for professional users and only trained, authorized personnel are permitted to operate, service and maintain the products. This personnel must be specifically informed about the possible hazards. The product and its ancillary equipment can present hazards if used incorrectly by untrained personnel or if used not in accordance with the intended use.
 products are designed for professional users and only trained, authorized personnel are permitted to operate, service and maintain the products. This personnel must be specifically informed about the possible hazards. The product and its ancillary equipment can present hazards if used incorrectly by untrained personnel or if used not in accordance with the intended use.
   The type designation and serial number are printed on the rating plate.
- Write down the serial number in the table below. You will be required to state the product details when contacting Hilti Service or your local Hilti organization to inquire about the product.
 Product informationLaser range meter PD-E Generation 01 Serial no. 
Laser information on the product
Laser informationLaser information
|  | Laser Class 2 based on the IEC60825-1 / EN60825-1:2007 standard in compliance with CFR 21 § 1040 (Laser Notice 50). | 
|  | Laser Class 2: Do not stare into the beam. Do not direct the beam toward other persons or toward areas in which other persons, who are not involved in the work with lasers, may be present. | 
|  | Recycle waste material. | 
Declaration of conformity
 
    The technical documentation is filed here:
Hilti Entwicklungsgesellschaft mbH | Tool Certification | Hiltistrasse 6 | D-86916 Kaufering, Germany
Safety
Safety instructions
Basic information concerning safety
In addition to the safety rules listed in the individual sections of these operating instructions, the following rules must be strictly observed at all times. The product and its ancillary equipment may present hazards when used incorrectly by untrained personnel or when used not as directed.- Keep all safety instructions and information for future reference.
- Stay alert, watch what you are doing and use common sense when working with the product. Do not use the product while you are tired or under the influence of drugs, alcohol or medication. A moment of inattention while operating the product may result in serious personal injury.
- Do not render safety devices ineffective and do not remove information and warning notices.
- If the product is opened improperly, laser radiation in excess of Class 2 may be emitted. Have the product repaired only by Hilti Service. 
- Tampering with or modification of the product is not permitted.
- Check that the product functions correctly each time before use.
- Measurements taken through panes of glass or other objects may be inaccurate.
- The measurement may be incorrect if the conditions under which the measurement is taken change rapidly, e.g. due to people walking through the path of the laser beam.
- Do not point the product toward the sun or other powerful light sources.
- Take the influences of the surrounding area into account. Do not use the tool where there is a risk of fire or explosion.
- Observe the information printed in the operating instructions concerning operation, care and maintenance.
General safety rules
- Check the product for damage before use. Have the damage repaired by Hilti Service.
- Check the accuracy of the product after it has been dropped or subjected to other mechanical stresses.
- Although the product is designed for the tough conditions of jobsite use, as with other measuring instruments it should be treated with care.
- Products which are not in use must be stored in a dry, high place or locked away out of reach of children.
- The product is not intended for use by children.
- Observe the national health and safety requirements.
Proper preparation of the working area
- Avoid unfavorable body positions when working from ladders. Make sure you have a safe stance and that you stay in balance at all times.
- Secure the site at which you are taking measurements and take care to avoid directing the laser beam toward other persons or toward yourself.
- When the product is brought into a warm environment from very cold conditions, or vice-versa, allow it to become acclimatized before use.
- Use the product only within its specified limits.
- Keep the laser exit window clean in order to avoid measurement errors.
- Observe the accident prevention regulations applicable in your country.
Working safely with laser tools
- Laser Class 2/Class II tools may be operated only by appropriately trained persons.
- Laser beams should not be projected at eye height.
- Precautions must be taken to ensure that the laser beam does not unintentionally strike highly reflective surfaces.
- Precautions must be taken to ensure that persons do not stare directly into the beam.
- The laser beam must not be allowed to project beyond the controlled area.
- Switch the laser tool off when it is not in use.
- Store laser tools, when not in use, in places to which unauthorized persons have no access.
Electromagnetic compatibility
Although the device complies with the strict requirements of the applicable directives, Hilti cannot entirely rule out the possibility of interference to the device caused by powerful electromagnetic radiation, possibly leading to incorrect operation. Check the accuracy of the device by taking measurements by other means when working under such conditions or if you are unsure. Likewise, Hilti cannot rule out the possibility of interference with other devices (e.g. aircraft navigation equipment). The tool complies with the requirements of class A; The possibility of interference occurring in a domestic environment cannot be excluded.Only for Korea: This laser range meter is suitable for commercial and industrial use and for the electromagnetic radiation encountered in this field (Class A). Users must pay attention to this point and make sure that this laser range meter is not used in occupied living areas.
Description
Overview of the product
 
     - Rear contact surface
- Reference indicator LED for rear contact
- Left arrow button
- Menu button
- “Measure” button
- Graphic display
- Reference indicator LED for front contact
- Side “Measure” button
- On/off button
- Right arrow button
- Hand strap attachment point
- Delete (clear) button
- ¹/₄ inch thread
- Folding spike
- Laser emitting and receiving lens
- Optical sight
- ¹/₄ inch thread
Intended use
The product described is a laser range meter. It is designed for taking individual measurements as well as the continuous measurement of distances.
Distances can be measured from all stationary targets without a highly reflective surface, i.e. concrete, stone, wood, plastic, paper, etc. The use of prisms or other highly reflective targets is not permissible and, if attempted, may falsify the results.The product is approved for use with batteries of the type AAA.
Explanation of the display
Main menu|  | Select angle unit | 
|  | Determine painter’s area | 
|  | Single Pythagoras | 
|  | Measure areas and volumes | 
|  | Select special functions | 
|  | Select trapezoid function | 
|  | Select Pythagoras function At least one right angle is required for horizontal and diagonal distances. | 
|  | Select settings | 
|  | Measure indirectly No specific angle is required for measurements on non-moving objects such as walls. | 
|  | Battery charge state | 
|  | Measuring spike not folded out | 
|  | Measuring spike folded out | 
|  | Measure | 
|  | Add distances | 
|  | Subtract distances | 
|  | Select | 
|  | Do not select | 
|  | Select measuring time | 
|  | Select calculator | 
|  | Inclination in percent | 
|  | Metric units | 
|  | Imperial units | 
|  | Inclination in angular degrees | 
|  | Measure rectangular areas | 
|  | Measure triangular areas | 
|  | Measure volumes | 
|  | Measure cylinder volume | 
|  | Select outdoor mode | 
|  | Select automatic brightness sensor | 
|  | Determine area to be painted | 
|  | Select layout function | 
|  | Select min/max delta function | 
|  | Select timer | 
|  | Select offset function | 
|  | Select data storage media | 
|  | Measure 3 distances | 
|  | Measure 2 distances, 1 angle | 
|  | Single Pythagoras | 
|  | Double Pythagoras | 
|  | Combined Pythagoras | 
|  | Unit of measurement. Select unit of measurement:  meter  centimeter  millimeter | 
|  | Measuring references. Select measuring reference:  front edge  rear of thread  underside of thread | 
|  | Angle unit. Select angle unit:  inclination in percent  metric units  imperial units  inclination in angular degrees | 
|  | Select expert mode | 
|  | Edit favorites list | 
|  | Activate scale | 
|  | Switch signal tone on / off | 
|  | Select laser on constantly | 
|  | Select automatic brightness sensor | 
|  | Calibrate inclination sensor | 
|  | Display information about the tool | 
|  | Reset to default settings | 
|  | Indirect horizontal distance measurement | 
|  | Indirect vertical distance measurement | 
|  | Take measurements on ceilings | 
|  | Indirect vertical distance measurement II | 
Items supplied
Laser range meter, two batteries, operating instructions, manufacturer’s certificate.Technical data
| Rated voltage | 3 V | 
| Rated current | 400 mA | 
| Maximum site elevation above datum | 2,000 m (6,561 ft - 10 in) | 
| Maximum relative humidity | 80 % | 
| Operating temperature | −10 ℃ … 50 ℃ (14 ℉ … 122 ℉) | 
| Distance measurement accuracy (2σ, standard deviation) | ±1.0 mm | 
| Inclination measurement accuracy (2σ, standard deviation) | ±0.2° | 
| Output power, laser | < 1 mW | 
| Wavelength, laser | 639 nm (0.0000252 in) | 
| Pulse duration | < 3.6 ns | 
| Pulse period | 8.3 ns … 243 ns | 
| Weight (including batteries) | 165 g (5.8 oz) | 
| Storage temperature | −30 ℃ … 70 ℃ (−22 ℉ … 158 ℉) | 
| Laser class in accordance with EN 60825-1:2007 | Laser class 2 | 
| Protection class in accordance with IEC 60529 | IP 65 | 
Operation
Basic functions
Navigate to the desired function with the aid of the left or right arrow buttons.- Always press the “Measure” button to select a function.
Inserting the batteries
 
    - Open the battery compartment and insert the batteries.
Switching the laser range meter on and off
- If the tool is switched off, press the on/off button or the “Measure” button to switch it on.
- If the tool is switched on, press the on/off button to switch it off.
Measuring using the spike
 
    - Fold out the spike through 90°. The spike can then be used as the contact point.
 
- Fold out the spike through 180°. The measuring reference point is then set automatically.
Measuring using a target plate
 
    - Use the target plate to measure distance under the following unfavorable conditions:
 - The wall is not sufficiently reflective due to the type of surface.
 - The target point is not on a surface.
 - The distance to be measured is very long.
 - The light conditions are unfavorable (bright sunshine).
 
- The wall is not sufficiently reflective due to the type of surface.
- A distance of 1.2 mm should be added to the measured distance when using a target plate.
Measurement mode
Single measurements
- Press the “Measure” button briefly to activate the laser beam.
- Keep the laser beam on the target point.
- Press the “Measure” button briefly to take the measurement.
 - The measured distance is shown in the lower line of the display.
 - The distance measured in the previous measurement is shown in the upper line of the display.
 
- The measured distance is shown in the lower line of the display.
- To take another measurement, keep the laser beam on the target point and press the “Measure” button again.
Continuous measurement
- Press the “Measure” button for 2 seconds.
 - If the signal tone is active, a signal tone will be emitted.
 
- If the signal tone is active, a signal tone will be emitted.
- Move the laser range meter toward or away from the target until the desired distance is reached.
- Press the “Measure” button briefly.
 - The measured distance is shown in the lower line of the display.
 - The distance measured in the previous measurement is shown in the upper line of the display.
 
- The measured distance is shown in the lower line of the display.
Selecting the angle unit
- Select the angle unit symbol from the menu.
- Navigate to the desired angle unit with the aid of the left or right arrow buttons.
- Select the desired angle unit by pressing the “Measure” button.
Measuring areas and volumes
Measuring rectangular areas
- Aim the tool at the target point for the room width and press the “Measure” button.
- Aim the tool at the target point for the room length and press the “Measure” button.
Measuring triangular areas
- Aim the tool at the target point and press the “Measure” button.
- Aim the tool at the target point and press the “Measure” button.
- Aim the tool at the third target point and press the “Measure” button.
Measuring volumes
- Aim the tool at the target point and press the “Measure” button.
- Aim the tool at the next target point and press the “Measure” button.
- Aim the tool at the next target point and press the “Measure” button.
Measuring cylindrical volume
- Aim the tool at the corresponding target to measure the height of the cylinder and press the “Measure” button.
- Aim the tool at the next target point to measure the diameter of the cylinder and press the “Measure” button.
Special functions
Automatic brightness sensor
- Select the symbol for the automatic brightness sensor from the special functions menu.
 
Painter’s area
- Aim the tool at the target point for the first room length and press the “Measure” button.
 - The result is saved as an intermediate result.
 
- The result is saved as an intermediate result.
- Aim the tool at the target for the next room length and press the “Measure” button to take the measurement.
 - The second result is shown in the intermediate results table. The intermediate result shown in bold is the sum of the measured room lengths.
 
- The second result is shown in the intermediate results table. The intermediate result shown in bold is the sum of the measured room lengths.
- Repeat this procedure until all room lengths have been measured.
- Press the right arrow button to switch to room height and confirm by pressing the “Measure” button.
- Position and aim the tool for room height measurement and then take the measurement.
 - The room height is measured and displayed in the intermediate result line. The painter’s area is calculated immediately and shown in the result line.
 
- The room height is measured and displayed in the intermediate result line. The painter’s area is calculated immediately and shown in the result line.
Layout function
- Enter the distance manually. Do this by using the left or right arrow buttons to select the keyboard symbol and confirm by pressing the “Measure” button.
- Select the applicable numbers and confirm by pressing the “Measure” button.
- To confirm the value, select the check mark symbol (tick) at the bottom right corner.
- Select the flag symbol.
 - The distance you have entered will then be shown between the two flags.
 
- The distance you have entered will then be shown between the two flags.
- Press the “Measure” button to begin measuring.
 - The arrows on the screen indicate in which direction you must move the tool. When the target distance is reached, black arrows appear above and below the distance shown in the display.
 
- The arrows on the screen indicate in which direction you must move the tool. When the target distance is reached, black arrows appear above and below the distance shown in the display.
- To repeat this distance measurement several times, move the tool further. The number of times you have measured out this distance is shown on the right of the screen.
- Press the “Measure” button to stop measuring.
 
Min/max delta function
- Select the symbol for the min/max delta function from the special functions menu.
- Aim the tool at the target point and press the “Measure” button.
- Press the “Measure” button to stop measuring.
 - The last distances measured are shown in the results line.
 
- The last distances measured are shown in the results line.
Data storage
- Select the data storage symbol from the special functions menu.
 
- To delete data storage memory, press and hold the C-button for 2 seconds while the data storage screen is displayed.
Trapezoid
Trapezoid function (3 distances)
- Select the symbol for the trapezoid function for 3 distances from the trapezoid functions menu.
- Aim the tool at the target point and press the “Measure” button.
 - After measuring the first distance, the graphical display automatically prompts you to take the next measurement.
 
- After measuring the first distance, the graphical display automatically prompts you to take the next measurement.
- Aim the tool at the next target point and press the “Measure” button.
- Aim the tool at the third target point and press the “Measure” button.
Trapezoid with inclination (2 distances, 1 angle)
- Select the symbol for the trapezoid function with inclination from the trapezoid functions menu.
- Aim the tool at the target point and press the “Measure” button.
- Aim the tool at the next target point and press the “Measure” button.
Pythagoras
Single Pythagoras
- Aim the tool at the target point and press the “Measure” button.
- Aim the tool at the next target point and press the “Measure” button.
 
Double Pythagoras
- Aim the tool at the target point and press the “Measure” button.
- Aim the tool at the next target point and press the “Measure” button.
 
- Aim the tool at the third target point and press the “Measure” button.
Combined Pythagoras
- Aim the tool at the target point and press the “Measure” button.
- Aim the tool at the next target point and press the “Measure” button.
- Aim the tool at the next target point and press the “Measure” button.
Settings
Editing the favorites list
- Navigate to the function that you wish to edit and confirm by pressing the “Measure” button.
- Navigate to the desired function and confirm by pressing the “Measure” button.
Activating the scale
- Set the applicable number and confirm the value by pressing the “Measure” button.
- Select the check mark symbol (tick) to confirm the value.
Calibrate inclination sensor
- Place the tool on a horizontal surface and press the “Measure” button.
- Rotate the tool through 180° and press the “Measure” button.
 - The inclination sensor is now calibrated.
 
- The inclination sensor is now calibrated.
Indirect measurements
Indirect horizontal distance measurement
- Aim the tool at the target point and press the “Measure” button.
 - The distance and angle of inclination are measured and shown in the intermediate result line.
 - The target distance is calculated immediately and shown in the result line.
 
- The distance and angle of inclination are measured and shown in the intermediate result line.
Indirect vertical distance (2 angles, 2 distances)
- Aim the tool at the target point and press the “Measure” button.
 - The first distance and angle are measured and shown in the intermediate result line.
 - The graphical display automatically prompts you to measure the second distance.
 
- The first distance and angle are measured and shown in the intermediate result line.
- Aim the tool at the next target point and press the “Measure” button.
 - The target distance is calculated immediately and shown in the result line.
 
- The target distance is calculated immediately and shown in the result line.
Taking measurements on ceilings
- Aim the tool at the target point and press the “Measure” button.
 - The first distance and angle are measured and shown in the intermediate result line.
 - The graphical display automatically prompts you to measure the second distance.
 
- The first distance and angle are measured and shown in the intermediate result line.
- Aim the tool at the next target point and press the “Measure” button.
 - The target distance is calculated immediately and shown in the result line.
 
- The target distance is calculated immediately and shown in the result line.
Indirect vertical distance II (2 angles, 1 distance)
- Aim the tool at the target point and press the “Measure” button.
 - The first distance and angle are measured and shown in the intermediate result line.
 - The graphical display automatically prompts you to measure the second distance.
 
- The first distance and angle are measured and shown in the intermediate result line.
- Aim the tool at the next target point and press the “Measure” button.
 - The target distance is calculated immediately and shown in the result line.
 
- The target distance is calculated immediately and shown in the result line.
Care, transport and storage
Cleaning
- Do not touch the lens with the fingers.
- Clean the lens by blowing the dust off or by wiping with a clean, dry cloth.
- Do not use liquids other than pure alcohol or water.
Transport
- Use the Hilti packaging or packaging of equivalent quality for transporting or shipping your equipment.
Storage and drying
- Do not put the product into storage when wet. Allow it to dry before putting it away.
- Observe the temperature limits given in the Technical Data section which are applicable to storage or transport of the equipment.
- Check the accuracy of the equipment before it is used after a long period of storage or transportation.
Disposal
 Most of the materials from which 
  Hilti products are manufactured can be recycled. The materials must be correctly separated before they can be recycled. In many countries, your old tools, machines or appliances can be returned to 
  Hilti for recycling. Ask 
  Hilti Service or your Hilti representative for further information.
 Most of the materials from which 
  Hilti products are manufactured can be recycled. The materials must be correctly separated before they can be recycled. In many countries, your old tools, machines or appliances can be returned to 
  Hilti for recycling. Ask 
  Hilti Service or your Hilti representative for further information.
  In accordance with the European Directive on waste electrical and electronic equipment and its implementation in conformance with national law, electric tools or appliances that have reached the end of their life must be collected separately and returned to an environmentally compatible recycling facility.
Manufacturer’s warranty
- Please contact your local Hilti representative if you have questions about the warranty conditions.