SI‑AT‑A22
 Original operating instructions
Information about the documentation
About this documentation
- Read this documentation before initial operation or use. This is a prerequisite for safe, trouble-free handling and use of the product.
- Observe the safety instructions and warnings in this documentation and on the product.
- Always keep the operating instructions with the product and make sure that the operating instructions are with the product when it is given to other persons.
Explanation of symbols used
Warnings
Warnings alert persons to hazards that occur when handling or using the product. The following signal words are used:Symbols in the documentation
The following symbols are used in this document:|  | Read the operating instructions before use. | 
|  | Instructions for use and other useful information | 
|  | Dealing with recyclable materials | 
|  | Do not dispose of electric equipment and batteries as household waste | 
Symbols in the illustrations
The following symbols are used in illustrations:|  | These numbers refer to the corresponding illustrations found at the beginning of these operating instructions | 
|  | The numbering reflects the sequence of operations shown in the illustrations and may deviate from the steps described in the text | 
|  | Item reference numbers are used in the overview illustrations and refer to the numbers used in the product overview section | 
|  | This symbol is intended to draw special attention to certain points when handling the product. | 
Product-dependent symbols
Symbols on the product
The following symbols are used on the product:|  | Direct current (DC) | 
Product information
 products are designed for professional users and only trained, authorized personnel are permitted to operate, service and maintain the products. This personnel must be specifically informed about the possible hazards. The product and its ancillary equipment can present hazards if used incorrectly by untrained personnel or if used not in accordance with the intended use.
 products are designed for professional users and only trained, authorized personnel are permitted to operate, service and maintain the products. This personnel must be specifically informed about the possible hazards. The product and its ancillary equipment can present hazards if used incorrectly by untrained personnel or if used not in accordance with the intended use.
   The type designation and serial number are printed on the rating plate.
- Write down the serial number in the table below. You will be required to state the product details when contacting Hilti Service or your local Hilti organization to inquire about the product.
 Product informationType SI‑AT‑A22 Generation 01 Serial no. 
Safety
Safety precautions
- Observe the safety precautions in the operating instructions for the wrench.
Description
Adaptive torque module
 
     - Control panel buttons
- Liquid crystal display
- Indicator LEDs
- Barcode scanner
- Release button
- USB port
- USB port cover (shown open in the illustration)
Control panel buttons
 
     - OK button
- Left arrow button
- Right arrow button
- Lock button
- Scan button
Intended use
The product described is an electronic module that can be used with Hilti impact wrenches of the types SI… …AT‑A22 ("…" = any character) to tighten threaded fasteners under controlled conditions, thereby safeguarding the quality of the bolted connection. A record of the work carried out is saved in the module and can be read out, for documentation purposes, using the AT Documentation Software PC application.
It is not possible to set a torque with this module!- Use only Hilti lithium‑ion batteries of the B 22 series with this product. 
- Use only Hilti -approved battery chargers to charge these batteries. More information is available from your Hilti Store or from www.hilti.group 
- Use only the impact sockets described in the operating instructions of the relevant product to tighten Hlti fasteners. 
Possible misuse
This product is not suitable for Hilti fasteners in nuclear power plants!Indicator LEDs
The LEDs on each side of the module indicate the following:| Status | Meaning | 
|---|---|
| The LEDs show green. | 
 
 | 
| The LEDs flash red. | 
 
 | 
| The LEDs flash yellow. | The module detected that the threaded fastener had been tightened and subsequently slackened. Consequently, the threaded fastener has been retightened in accordance with defined parameters for retightening, and the tightening operation has been completed successfully. | 
Buzzer
The buzzer in the adaptive torque module emits the following signal tones as audible feedback:- Long buzz: Confirmation signal (OK / operation completed successfully)
- 2 short buzzes, the LEDs flash yellow: Warning 1 (OK or, as applicable, not OK / repeat tightening)
- 4 short buzzes, the LEDs flash red: Warning 2 (not OK / operation aborted)
USB connection
The USB port can be used to connect the adaptive torque module to a PC. When this connection is made, the AT Documentation Software offers a range of functions, including:- Adding new data records for new fasteners
- Changing / updating existing data records
- Deactivating / activating the documentation function
- Loading the log from the documentation function
- Setting the clock in the torque module
Items supplied
Adaptive torque module, operating instructions, quick-start guide, USB cable.Other system products approved for use with this product can be found at your local Hilti Store or at: www.hilti.group
Technical data
| Weight | 0.57 lb (0.26 kg) | 
| Bar code scanner | Camera / scanner (imager) | 
Operation
Inserting the adaptive torque module
 
    - Push the torque module on to the impact wrench from the rear until it engages with an audible click.
Inserting the battery
 
    - Push the battery on to the torque module from the rear until it engages with an audible click.
Switching on and off
Switching on the torque module
Conditions : The torque module is switched off, the display is blank.- Set the forward/reverse switch on the impact wrench to the "forward" position.
- Short-press the control switch on the impact wrench.
 - The display lights up and briefly shows the  start screen. start screen.
 - As a function check the LEDs briefly show red and yellow, before turning green. An acoustic signal sounds.
 - The last operating mode selected appears inside a selection frame on the display.
 - If the display shows a fault:
 - Refer to the "Troubleshooting”" section for information about possible causes of error messages and the steps to be taken to rectify the problem.
 
- Refer to the "Troubleshooting”" section for information about possible causes of error messages and the steps to be taken to rectify the problem.
 
- The display lights up and briefly shows the 
- Press the lock button.
 - The torque module is now locked and the impact wrench is ready for use.
 
- The torque module is now locked and the impact wrench is ready for use.
Switching off the torque module
The adaptive torque module switches itself off automatically:- when the impact wrench switches off automatically after a long idle period
- when the battery is removed
- when a USB connector is unplugged, interrupting the USB connection between the torque module and the PC.
Basic operation
Unlocking the moduleThe adaptive torque module has to be unlocked before changes can be made to the settings.- To unlock the adaptive torque module, press the   lock button and hold it down for at least 1 second. lock button and hold it down for at least 1 second.
- In the display a selection frame appears around the last previously shown type of fastener and the last previously shown operating mode.
- The torque module is unlocked and in setting mode. The impact wrench is deactivated.
 and
 and 
    .
.
   Selecting options / changing parametersWhen the torque module is unlocked, you can change options or parameters as described below.
- Position the selection frame in the display on the element (option / parameter) you want to change.
- Press the OK button.
- A black background appears behind the element.
- Use the arrow buttons to select the setting you want.
- Press the OK button to accept the setting.
- The element reappears surrounded by the selection frame.
- Press the lock button  . .
- The selection frame disappears. Your operating parameters settings have now been saved and cannot be changed accidentally.
- The adaptive torque module is locked and the impact wrench is reactivated.
Basic settings
Calling up the "Basic settings" menu
- If it is locked, unlock the torque module by pressing the lock button and holding it down for at least 1 second.
- Press the OK button and hold it down for at least 1 second.
 - The "Basic settings" menu appears on the display.
 
- The "Basic settings" menu appears on the display.
Selecting functions from the basic settings menu
- Use the arrow buttons to move the selection frame to the symbol for the desired function.
 Functions in the "Basic settings" menuSymbol Function  Show the date and time set in the torque module's clock 
  Show the remaining time / period of use until servicing of the impact wrench is due  Show the percentage of memory used in the torque module 
  Show the version of the software installed in the torque module  Exit the "Basic settings" menu 
- Press the OK button.
Display showing maintenance status / remaining period of use
After activation of the symbol in the basic settings menu the remaining period of use of the impact wrench until the next service is shown in the following display screens.
 symbol in the basic settings menu the remaining period of use of the impact wrench until the next service is shown in the following display screens.
   Display icons for maintenance status of the impact wrench
| Display | Meaning | 
|---|---|
|  | The impact wrench is in good condition, no maintenance required in the foreseeable future. | 
|  | Maintenance of the impact wrench will soon be due. The segments in the rectangle on the right in the display indicate residual usage period. | 
|  | Maintenance of the impact wrench must be carried out immediately. This warning appears automatically when the residual usage period expires. The "Adaptive" and "Tightening" operating modes can no longer be selected. | 
Leaving the basic settings menu
- Move the selection frame to the  symbol. symbol.
- Press the OK button.
 - The last previously shown operating mode will be displayed.
 
- The last previously shown operating mode will be displayed.
Operating modes
Adaptive operation
In this operating mode the adaptive torque module regulates the tightening of the selected type of threaded fastener. The tightening parameters from the most recently installed software update are used. Product designations and tightening parameters can change, so it essential to ensure that the software version installed in the torque module is always up to date.- When the "Adaptive" operating mode is selected, the impact wrench's "AT" torque indicator lights up.
- The switch for selecting the operating stage is not active. But you can use the control switch to turn the impact wrench ON and OFF.
 Follow the operating instructions for your impact wrench.
 
     - Type of threaded fastener (short name for fastener)
- Material grade / quality
- Diameter (optional)
Type of threaded fastenerParameters for various types of threaded fastener are saved ex-works in the torque module.
The fastener shown must correspond to the fastener used.
Further information can be found in the quick-start guide of the SI-AT-A22 and in the operating instructions of the product you use.
"Tightening" operating mode
In this operating mode a total of 30 torque settings are available. The setting to be selected for a particular type of fastener depends on the diameter of the fastener and the specified torque. The setting has to be determined step by step on the basis of these data.For the "Tightening" operating mode, the display shows the following:
 
    Determining the required setting for the "Tightening" operating mode
 ATTENTION: Before starting to tighten a threaded fastener, always check that the mating faces of the components to be joined are seated flat against each other and that the nut has been screwed down until it is seated against the component. ATTENTION: Before starting to tighten a threaded fastener, always check that the mating faces of the components to be joined are seated flat against each other and that the nut has been screwed down until it is seated against the component.
- Use a low setting for initial tightening of the fastener.
 - Start the step-by-step process with as low a setting as possible, to avoid the possibility of overtightening and damaging the fastener.
 
- Start the step-by-step process with as low a setting as possible, to avoid the possibility of overtightening and damaging the fastener.
- Use a calibrated torque wrench to check the torque applied to the fastener.
 Result 1 / 3The specified tightening torque of the fastener to be tightened was not achieved.
 - Back off the fastener and set the torque module to a higher stage.
 - Tighten the fastener with the new stage setting and repeat this test step.
 
 - Back off the fastener and set the torque module to a lower stage.
 - Tighten the fastener with the new stage setting and repeat this test step.
 
 This stage setting is correct for this fastener.
- Back off the fastener and set the torque module to a higher stage.
"Unregulated" operating mode
In this operating mode the adaptive torque module is deactivated. The impact wrench works as though the adaptive torque module were not fitted to the tool. The adaptive torque module therefore does not have to be actually removed when it is not needed for short periods of use.In the "Unregulated" operating mode the display shows the following:
 
    Setting the operating mode
There are 2 ways of setting the operating mode to suit the type of fastener:- Scan the barcode or QR code on the packaging of the Hilti product you are going to tighten.
- Manual adjustment using the buttons on the torque module
Manual adjustmentIf no barcode or QR code is available for the product to be tightened, the operating mode can be set by using the buttons on the torque module.
Setting the operating mode with the control panel buttons
- Unlock the torque module.
- Use the arrow buttons to move the selection frame, as necessary, to the option you want to change.
- Press the OK button.
 - A black background appears behind the option you selected.
 
- A black background appears behind the option you selected.
- Use the arrow buttons to select the desired setting.
- Press the OK button.
 - The selected setting appears in the selection frame.
 
- The selected setting appears in the selection frame.
- Repeat the last 3 steps as necessary to make other changes.
- Lock the torque module.
Setting the operating mode by scanning the barcode or QR code
- Unlock the torque module.
- Press the "Scan" button.
 - The scanner is activated and the  symbol appears on the display to indicate that the scanner is ready. symbol appears on the display to indicate that the scanner is ready.
 
- The scanner is activated and the 
 
    - Hold the module facing the barcode or QR code at a distance of approx. 15 centimeters (6″), so that the code is inside the frame projected by the scanner.
 - The LEDs show green. 
 - The confirmation tone sounds.
 - The operating mode for the product to be tightened appears on the display.
 - The LEDs flash red.
 - The warning tone sounds.
    appears on the display (code could not be read or was not recognized). appears on the display (code could not be read or was not recognized).
 - Press the "Scan" button and scan the code again.
 
 
- Press the "Scan" button and scan the code again.
 
- The LEDs show green. 
Tightening the threaded fastener in "Adaptive" operating mode
- Select the "Adaptive" operating mode.
- Set the forward/reverse switch to the "Forward" position.
- Install a suitable accessory tool on the impact wrench and engage the product to be tightened.
- Press the control switch and hold it down until the torque module returns one of the following feedback signals:
 
    - The symbol indicating "Tightening completed successfully" is displayed.
- The LEDs show green.
- The confirmation tone sounds.
 
    - The symbol indicating "Retightening completed successfully" is displayed.
- The LEDs flash yellow.
- The warning tone sounds.
 
    - The symbols indicating "Battery voltage too low" are displayed.
- The LEDs flash red.
- Press the OK button to confirm the message.
- Insert a charged battery.
 
    - The symbols indicating "Tightening not completed correctly" are displayed.
- The LEDs flash red.
- The warning tone sounds.
- Use a calibrated torque wrench to apply the correct tightening torque to the fastener.
Tightening the threaded fastener in "Tightening" operating mode
- Select the "Tightening" operating mode.
- Determine the tightening setting for the threaded fastener to be tightened and select this setting.
- Set the forward/reverse switch to the "Forward" position.
- Install a suitable accessory tool on the impact wrench and engage the product to be tightened.
- Press the control switch and hold it down until the torque module returns one of the following feedback signals:
 
    - The symbol indicating "Tightening completed successfully" is displayed.
- The LEDs show green.
- The confirmation tone sounds.
 
    - The symbols indicating "Tightening not completed correctly" are displayed.
- The LEDs flash red.
- The warning tone sounds.
- Use a calibrated torque wrench to apply the correct tightening torque to the fastener.
Checking fastener
All Hilti products are subject to a process of constant updating, which means that products not described in this documentation might also be supported by the SI-AT module. Keep the software and the operating instructions up to date at all times.Other system products approved for use with this product, the latest operating instructions and instructions for testing can be found online at: www.hilti.group | USA: www.hilti.com .
Checking the fasteners of stud anchors
- Use a calibrated torque wrench to apply additional torque to the nut of the stud anchor. In this process, observe the angle through which the fastening element can be turned in the tightening direction.
 Result 1 / 2The nut of the stud anchor was not turned further than through the specified maximum angle of rotation (< 180 °).
 The fastener was tightened correctly.
 Result 2 / 2The nut of the stud anchor was turned further than the specified maximum angle of rotation (> 180 °).
 The fastener was not tightened correctly. The threaded fasteners tightened since the previous check are to be regarded as faulty and must be checked. Have the impact wrench checked by Hilti Service.
Checking security of the fastener for installation systems
- Use a calibrated torque wrench to apply additional torque to the fastener. In this process, observe the angle through which the fastening element can be turned in the tightening direction.
 Result 1 / 2The fastener was not turned further than through the specified maximum angle of rotation (< 180 °).
 The fastener has been tightened correctly.
 Result 2 / 2The fastener was turned further than the specified maximum angle of rotation (> 180 °).
 The threaded fastener has not been installed correctly. The threaded fasteners tightened since the previous check are to be regarded as faulty and must be checked. Have the impact wrench checked by Hilti Service.
Checking threaded fasteners tightened in the "Tightening" operating mode
- At regular intervals, using a calibrated torque wrench and proceeding in accordance with company regulations or quality specifications, check that specified tightening torque has been achieved.
Removing the torque module
 
    - Remove the battery.
- Press and hold down the release button of the torque module.
- Pull the torque module to the rear and off the impact wrench.
Connecting the torque module to a PC
 
    - Remove the torque module.
- Open the sliding cover on the underside of the torque module.
 - The USB port is accessible.
 
- The USB port is accessible.
- Plug the connector of the USB cable (type B, USB 2.0) into the USB port of the torque module.
- Plug the other connector of the USB cable (type A) into the PC.
 - The torque module is now powered off the PC. The USB logo  appears on the module's display. appears on the module's display.
 
- The torque module is now powered off the PC. The USB logo 
Care and maintenance
- Keep the product, especially its grip surfaces, clean and free from oil and grease. Do not use cleaning agents containing silicone.
- Clean the outer surfaces of the tool with a slightly damp cloth at regular intervals.
Transport and storage
- Prevent damage by transporting and storing the adaptive torque module in the storage box supplied for the purpose, or in the toolbox of the impact wrench.
Troubleshooting
If the problem you are experiencing is not listed in this table or you are unable to remedy the problem by yourself, please contact Hilti Service.| Malfunction | Possible cause | Action to be taken | 
|---|---|---|
|   | Torque module unlocked. | 
 | 
|   | The battery has overheated. | 
 | 
|   | Battery temperature is too low. | 
 | 
|   | The impact wrench has overheated. | 
 | 
|   | The battery does not have enough power left to tighten the fastener correctly. | 
 | 
|   | Current input is briefly too high. | 
 | 
|   | The button cell battery for the clock in the torque module is discharged. | 
 | 
|   | A device error has been detected. | 
 | 
|   | Documentation function deactivated (warning only). | 
 | 
|   | Usage of data memory in the torque module is indicated in percent. Note: When 100 % is reached, the oldest data will be overwritten! | 
 | 
Disposal
 Most of the materials from which 
  Hilti tools and appliances are manufactured can be recycled. The materials must be correctly separated before they can be recycled. In many countries, your old tools, machines or appliances can be returned to 
  Hilti for recycling. Ask 
  Hilti Service or your Hilti representative for further information.
 Most of the materials from which 
  Hilti tools and appliances are manufactured can be recycled. The materials must be correctly separated before they can be recycled. In many countries, your old tools, machines or appliances can be returned to 
  Hilti for recycling. Ask 
  Hilti Service or your Hilti representative for further information.
  Manufacturer’s warranty
- Please contact your local Hilti representative if you have questions about the warranty conditions.