SL 2-A12
SL 2-A22
 Original operating instructions
Information about the operating instructions
About these operating instructions
- Warning! Read and understand all accompanying documentation, including but not limited to instructions, safety warnings, illustrations, and specifications provided with this product. Familiarize yourself with all the instructions, safety warnings, illustrations, specifications, components, and functions of the product before use. Failure to do so may result in electric shock, fire, and/or serious injury. Save all warnings and instructions for future reference.
- The accompanying documentation corresponds to the current state of the art at the time of printing. Please always check for the latest version on the product’s page on Hilti’s website. To do this, follow the link or scan the QR code in this documentation, marked with the symbol  . .
- Ensure that these operating instructions are with the product when it is given to other persons.
Explanation of symbols used
Warnings
Warnings alert persons to hazards that occur when handling or using the product. The following signal words are used:Symbols in the documentation
The following symbols are used in this document:|  | Read the operating instructions before use. | 
|  | Instructions for use and other useful information | 
|  | Dealing with recyclable materials | 
|  | Do not dispose of electric equipment and batteries as household waste | 
Symbols in the illustrations
The following symbols are used in illustrations:|  | These numbers refer to the corresponding illustrations found at the beginning of these operating instructions | 
|  | The numbering reflects the sequence of operations shown in the illustrations and may deviate from the steps described in the text | 
|  | Item reference numbers are used in the overview illustrations and refer to the numbers used in the product overview section | 
|  | This symbol is intended to draw special attention to certain points when handling the product. | 
Product-specific symbols
Symbols
The following symbols are used on the product:|  | Do not look into the light source. | 
|  | The product supports wireless data transmission compatible with iOS and Android platforms. | 
|  | Hilti Li-ion battery type series used. Observe the information given in the section headed Intended use . | 
|  | Li-ion battery | 
|  | Never use the battery as a striking tool. | 
|  | Do not drop the battery. Never use a battery that has suffered an impact or is damaged in any other way. | 
Product information
 products are designed for professional users and only trained, authorized personnel are permitted to operate, service and maintain the products. This personnel must be specifically informed about the possible hazards. The product and its ancillary equipment can present hazards if used incorrectly by untrained personnel or if used not in accordance with the intended use.
 products are designed for professional users and only trained, authorized personnel are permitted to operate, service and maintain the products. This personnel must be specifically informed about the possible hazards. The product and its ancillary equipment can present hazards if used incorrectly by untrained personnel or if used not in accordance with the intended use.
   The type designation and serial number are printed on the rating plate.
- Write down the serial number in the table below. You will be required to state the product details when contacting Hilti Service or your local Hilti organization to inquire about the product.
 Product informationCordless lamp SL2-A12 | SL2-A22 Generation 01 Serial no. 
Declaration of conformity
 
    The technical documentation is filed here:
Hilti Entwicklungsgesellschaft mbH | Tool Certification | Hiltistrasse 6 | 86916 Kaufering, Germany
Safety
Important safety instructions
WARNING! READ ALL INSTRUCTIONS. Failure to follow all instructions listed below can result in electric shock, fire and/or serious injury. KEEP THESE INSTRUCTIONS IN A HANDY YET SECURE PLACE.Careful handling and use
- Use the product only when it is in perfect working order.
- Never tamper with or modify the product in any way.
- This device can be used by children 8 years of age or older and by persons with physical, sensory or mental disabilities or little relevant experience or know-how if they are supervised or have received instruction on the safe use of the device and the resulting hazards.
- Do not use the product where there is a risk of fire or explosion.
- Do not use the device outdoors.
- Do not use accessories not specifically intended and recommended for this power tool by the tool manufacturer. The fact that an accessory can be attached to your power tool does not necessarily mean that it can be used in safety.
- Replace the complete cordless lamp when the light source has reached the end of its life. The light source in this cordless lamp is not replaceable.
- Do not look into the beam and do not direct the beam toward other persons.
- Do not expose the device to rain or moisture. Water entering an electric device will increase the risk of electric shock.
Careful handling and use of batteries
- Observe the special guidelines applicable to the transport, storage and use of lithium-ion batteries.
- Do not expose batteries to high temperatures, direct sunlight or fire.
- Do not disassemble, crush or incinerate batteries and do not subject them to temperatures over 80 °C (176 °F).
- Do not use or charge batteries that have suffered mechanical impact, have been dropped from a height or show signs of damage. In this case, always contact your Hilti  Service .
- If the battery is too hot to touch it may be defective. Put the battery in a place where it is clearly visible and where there is no risk of fire, at an adequate distance from flammable materials. Allow the battery to cool down. If it is still too hot to touch after an hour, the battery is faulty. Contact Hilti Service .
Description
Product overview
- Multi-position hinge
- LED bezel
- LED
- Retractable hook
- Automatic switch
- 3-mode switch
- Grip
- Battery
- Battery release button
Intended use
The product described is a cordless lamp. It is intended for use as illumination on jobsites. Use the product in a dry environment only.
SL 2-A12Use only Hilti Li-ion batteries from the B 12 series with this product.
- Use only the Hilti battery chargers of the C 4/36 series with the CA-B12 charging adapter, or battery chargers of the C 4/12-50 series for charging these batteries. 
Use only Hilti Li‑ion batteries of the B 22 series with this product.
- Use only the Hilti battery chargers of the C4/36 series for charging these batteries. 
Charge state indicator
Lightly press (no more than until resistance is perceptible) either of the battery release buttons to check the charge state of the Li‑ion battery.| Status | Meaning | 
|---|---|
| 4 LEDs light up. | Charge state: 75 % to 100 % | 
| 3 LEDs light up. | Charge state: 50 % to 75 % | 
| 2 LEDs light up. | Charge state: 25 % to 50 % | 
| 1 LED lights up. | Charge state: 10 % to 25 % | 
| 1 LED flashes. | Charge state: < 10 % | 
3-mode switch
Use the 3-mode switch to set the brightness.| Status | Meaning | 
|---|---|
| Press once | The lamp lights with maximum brightness. | 
| Press twice | The lamp lights with medium brightness. | 
| Press three times | The lamp is off. | 
Items supplied
Cordless lamp, operating instructions.Other system products approved for use with this product can be found at your local Hilti Center or online at: www.hilti.com
Technical data
Technical data
| SL 2-A12 | SL 2-A22 | |
|---|---|---|
| Voltage | 10.8 V | 21.6 V | 
| Brightness | 500 lm | 500 lm | 
| Weight | 0.65 kg | 1.3 kg | 
Battery
| Battery operating voltage | 10.8 V | 
| Ambient temperature for operation | −17 ℃ … 60 ℃ | 
| Storage temperature | −20 ℃ … 40 ℃ | 
| Battery charging starting temperature | −10 ℃ … 45 ℃ | 
Battery
| Battery operating voltage | 21.6 V | 
| Ambient temperature for operation | −17 ℃ … 60 ℃ | 
| Storage temperature | −20 ℃ … 40 ℃ | 
| Battery charging starting temperature | −10 ℃ … 45 ℃ | 
Operation
Preparations at the workplace
Observe the safety instructions and warnings in this documentation and on the product.Inserting the battery
- Insert the battery and check that the battery is securely seated in the device.
Removing the battery
- Press both release buttons.
- Pull the battery to the rear and out of the product.
Pivoting the head of the lamp
- Pull out the retractable hook.
 
- Pivot the head of the lamp upwards.
Turning the lamp head
- Turn the lamp head to the desired position.
 
Switching on
- Turn the lamp head to the desired position.
- Select a mode by pressing the 3-mode switch.
Care and maintenance
Care and maintenance
Care of the product- Carefully remove stubborn dirt.
- Carefully clean the air vents, if present, with a dry, soft brush.
- Use only a slightly damp cloth to clean the housing. Do not use cleaning agents containing silicone as these can attack the plastic parts.
- Use a dry, clean cloth to clean the contacts of the product.
- Never use a battery with clogged air vents. Clean the air vents carefully using a dry, soft brush.
- Avoid unnecessary exposure of the battery to dust and dirt. Never expose the battery to high levels of moisture (e.g. by being dipped in water or left in the rain).
 If a battery has been soaked by moisture, treat it as a damaged battery. Isolate it in a non-flammable container and consult Hilti Service.
- Keep the battery free of extraneous oil and grease. Do not permit dust or dirt to accumulate unnecessarily on the battery. Clean the battery with a dry, soft brush or a clean, dry cloth. Do not use cleaning agents containing silicone as these can attack the plastic parts.
 Do not touch the contacts of the battery and do not remove the factory-applied grease from the contacts.
- Use only a slightly damp cloth to clean the housing. Do not use cleaning agents containing silicone as these can attack the plastic parts.
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
- Never transport batteries loose and unprotected. During transport, batteries should be protected from excessive shock and vibration and isolated from any conductive materials or other batteries that may come in contact with the terminals and cause a short circuit. Comply with the locally applicable regulations for transporting batteries. 
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
If the trouble you are experiencing is not listed in this table or you are unable to remedy the problem by yourself, please contact Hilti Service.Troubleshooting
| Trouble or fault | Possible cause | Action to be taken | 
|---|---|---|
| The battery does not engage with an audible double click. | The retaining lugs on the battery are dirty. | 
 | 
| 1 LED flashes. The power tool does not work. | Battery is discharged. | 
 | 
| The battery is too hot or too cold. | 
 | 
Disposal
 Most of the materials from which Hilti products are manufactured can be recycled. The materials must be correctly separated before they can be recycled. In many countries, your old tools, machines or appliances can be returned to Hilti for recycling. Ask Hilti Service or your Hilti sales representative for further information.
 Most of the materials from which Hilti products are manufactured can be recycled. The materials must be correctly separated before they can be recycled. In many countries, your old tools, machines or appliances can be returned to Hilti for recycling. Ask Hilti Service or your Hilti sales representative for further information.
  RoHS (Restriction of Hazardous Substances)
 
    
   There is a link to the RoHS table, in the form of a QR code, at the end of this document.
Manufacturer’s warranty
- Please contact your local Hilti representative if you have questions about the warranty conditions.