VC 20 / VC 40
 Original operating instructions
Information about the documentation
About this documentation
- Read this documentation before initial operation or use. This is a prerequisite for safe, trouble-free handling and use of the product.
- Observe the safety instructions and warnings in this documentation and on the product.
- Always keep the operating instructions with the product and make sure that the operating instructions are with the product when it is given to other persons.
Explanation of symbols
Warnings
Warnings alert persons to hazards that occur when handling or using the product. The following signal words are used:
Symbols in the documentation
The following symbols are used in our documentation:
|  | Read the operating instructions before use | 
|  | Instructions for use and other useful information | 
|  | Dealing with recyclable materials | 
|  | Do not dispose of electric equipment and batteries as household waste | 
Symbols in the illustrations
The following symbols are used our in illustrations:
|  | These numbers refer to the corresponding illustrations found at the beginning of these operating instructions | 
|  | The numbering reflects the sequence of operations shown in the illustrations and may deviate from the steps described in the text | 
|  | Item reference numbers are used in the overview illustrations and refer to the numbers used in the product overview section | 
|  | This symbol is intended to draw special attention to certain points when handling the product. | 
|  | Wireless data transfer | 
Additional symbols
The following symbols are used on the product:
|  | Transport by crane is not permissible. | 
Product-dependent symbols
Symbols on the product
The following symbols are used on the product:
|  | Warning: hot surface | 
|  | Transport by crane is not permissible. | 
Special stickers on the product
Applicable to UL vacuum cleaners 
    WARNING: This unit contains hazardous dust. Emptying and maintenance, including the removal of the dust bag, may be carried out only by persons familiar with the unit and wearing suitable protective equipment. Do not switch on until the complete filter system has been installed.
Applicable to UM and UME vacuum cleaners 
    WARNING: This unit contains hazardous dust. Emptying and maintenance, including the removal of the dust bag, may be carried out only by well-informed persons wearing suitable protective equipment. Do not switch on the unit until the complete filter system has been installed and the function of the volume-flow control has been tested.
Product information
 products are designed for professional users and only trained, authorized personnel are permitted to operate, service and maintain the products. This personnel must be specifically informed about the possible hazards. The product and its ancillary equipment can present hazards if used incorrectly by untrained personnel or if used not in accordance with the intended use.
 products are designed for professional users and only trained, authorized personnel are permitted to operate, service and maintain the products. This personnel must be specifically informed about the possible hazards. The product and its ancillary equipment can present hazards if used incorrectly by untrained personnel or if used not in accordance with the intended use.
The type designation and serial number are printed on the rating plate.
- Write down the serial number in the table below. You will be required to state the product details when contacting Hilti Service or your local Hilti organization to inquire about the product.
 Product informationWet / dry vacuum cleaner VC 20-U | VC 20-UL | VC 20-UM | VC 20-UME 
 VC 40-U | VC 40-UL | VC 40-UM | VC 40-UMEGeneration 02 Serial no. 
Declaration of conformity
We declare, on our sole responsibility, that the product described here complies with the applicable directives and standards. A copy of the declaration of conformity can be found at the end of this documentation.
The technical documentation is filed here:
Hilti Entwicklungsgesellschaft mbH | Tool Certification | Hiltistrasse 6 | 86916 Kaufering, Germany
Safety
General safety instructions
In addition to the safety instructions given in the various sections of these operating instructions, the following points must be strictly observed at all times.
- Read all the instructions. Failure to follow all the instructions listed below may result in electric shock, fire and/or serious injury.
- If the appliance is used in conjunction with an electric tool, read and follow the operating instructions for the electric tool and all the warnings. 
- Modification of the appliance is not permitted. 
- Use the right appliance for the job. Do not use the appliance for purposes for which it was not intended. Use it only as directed and when in faultless condition. 
- Before beginning work with the appliance, find out how to operate it correctly and about any hazards associated with the materials it will be picking up and how these materials can be disposed of. 
- Take the influences of the surrounding area into account. Do not use the appliance where there is a risk of fire or explosion. 
- The appliance may only be used by persons who are familiar with it, have been trained on how to use it safely and who understand the resulting hazards. The appliance is not intended for use by children. 
- Store appliances in a secure place when not in use. When not in use, appliances must be stored in a dry, high place or locked away out of reach of children. 
Personal safety
- Stay alert, watch what you are doing and use common sense when working with the product.  Do not use the vacuum cleaner while you are tired or under the influence of drugs, alcohol or medication.  A moment of inattention while operating the appliance may result in serious personal injury.
- The user and any other persons in the vicinity must wear suitable eye protection, a hard hat, ear protection, protective gloves, safety footwear and breathing protection while the appliance is in use or while maintenance work on it is being carried out. 
- Engage the wheel brakes so that the vacuum cleaner stands securely. If the wheel brakes are disengaged the vacuum cleaner may run away out of control.
- If devices are provided for the connection of dust extraction and collection facilities, ensure these are connected and properly used. Use of a vacuum cleaner can reduce dust-related hazards.
Use and care of the appliance
- Never leave the appliance unattended. 
- Do not deactivate the filter cleaning system when picking up hazardous dusts, especially when the appliance is used in conjunction with electric tools that generate dust. 
- Protect the appliance from frost. 
- Clean the water level limiting device regularly with a brush, in accordance with the instructions, and check it for signs of damage. 
- When fitting the top section of the vacuum cleaner, take care to avoid pinching your fingers or damaging the supply cord. This presents a risk of injury or damage.
- Check the appliance and its accessories for any damage. Guards, safety devices and any slightly damaged parts must be checked carefully to ensure that they function faultlessly and as intended. Check that moving parts function faultlessly, without sticking, and that no parts are damaged. In order to ensure faultless operation of the appliance, all parts must be fitted correctly and must meet the necessary requirements. 
- Have the appliance serviced by a qualified repair person using only genuine Hilti spare parts. The safety of the appliance can thus be maintained.
- Always unplug the supply cord from the power outlet when the appliance is not in use (during breaks), before cleaning and maintenance and before changing the filter or accessories. This preventive safety measure reduces the risk of starting the appliance accidentally.
- Never pull the vacuum cleaner by the supply cord to a new working position. Do not run the wheels of the vacuum cleaner over the supply cord. 
- Do not transport the appliance by crane. 
- Close the hose inlet socket with the cap before transporting the appliance and when it is not in use. .
Electrical safety
- The plug on the supply cord of the appliance must match the outlet.  Do not change the plug in any way.  Do not use adapter plugs with earthed (grounded) appliances. Unmodified plugs and matching outlets reduce risk of electric shock.
- Insert the plug in a suitable earthed/grounded power outlet which has been correctly and safely installed and is in compliance with local regulations. If you are in doubt about the effectiveness of the power outlet’s earth/ground connection, have it checked by a qualified specialist. 
- Avoid body contact with earthed or grounded surfaces such as pipes, radiators, cookers, stoves and refrigerators. There is an increased risk of electric shock if your body is grounded.
- Do not expose the appliance to rain or wet conditions. Water entering an electric appliance will increase the risk of electric shock.
- Check to ensure that the supply cord does not lie in a puddle of water. 
- Check the appliance’s supply cord at regular intervals and have it replaced by Hilti Service if damage is found. Check extension cords at regular intervals and replace them if found to be damaged. 
- Do not touch the supply cord or extension cord if they are damaged while working.  Disconnect the supply cord plug from the power outlet. Damaged supply cords or extension cords present a risk of electric shock.
- The electric supply cord may be replaced only with a cord of the type specified in the operating instructions.
- Do not abuse the cord. Never use the cord for carrying, pulling or unplugging the appliance.  Keep the cord away from heat, oil, sharp edges or moving parts. Damaged or entangled cords increase the risk of electric shock.
- When operating an electric appliance outdoors, use only extension cords of a type suitable for outdoor use. Use of an extension cord suitable for outdoor use reduces the risk of electric shock.
- In the event of an interruption in the electric supply, switch the appliance off and unplug it from the power outlet. 
- Use the power outlet on the appliance only for the purposes described in the operating instructions. 
- Never operate the appliance when it is dirty or wet. Dust (especially dust from conductive materials) or dampness adhering to the surface of the appliance may, under unfavorable conditions, lead to electric shock. Dirty or dusty appliances should thus be checked by Hilti Service at regular intervals, especially if used frequently for working on conductive materials. 
Workplace
- Ensure that the workplace is well lit. 
- Ensure that the workplace is well ventilated. Exposure to dust at a poorly ventilated workplace may result in damage to the health.
- Keep the workplace tidy.  Objects which could cause injury should be removed from the working area. Untidiness at the workplace can lead to accidents.
- Do not operate the appliance in explosive atmospheres, such as in the presence of flammable liquids, gases or dust. Electric appliances cause sparks which may ignite the dust or fumes.
- Use extra care when working on stairs. 
The material picked up
- Do not use the appliance to pick up flammable or explosive dusts (magnesium or aluminum dust etc.) or dusts that present a health hazard. Do not use the appliance to pick up materials hotter than 60°C (140°F), (e.g. glowing cigarette ends, hot ash). 
- Do not use the appliance to pick up flammable, explosive or aggressive liquids (coolants and lubricants, gasoline, solvents, acids (pH < 5), alkalies (pH > 12.5), etc.). 
- Switch the appliance off immediately if foam or liquids escape from it. 
- Wear protective gloves when using the appliance to pick up hot materials at temperatures of up to 60°C (140°F). 
- When working with mineral drilling slurry, wear protective clothing and avoid skin contact with the slurry (pH > 9: caustic). 
- Avoid contact with alkaline or acidic liquids. If contact accidentally occurs, rinse with water. In the event of the liquid coming into contact with the eyes, rinse the eyes with plenty of water and consult a doctor. 
- A Dust Class L appliance is suitable for picking up dry, non-flammable dusts, liquids, wood chips and hazardous dusts with an exposure limit value of > 1 mg/m³. The appliance must be equipped with a suitable filter corresponding to the hazard classification of the dusts to be picked up. 
- A Dust Class M appliance is suitable for picking up dry, non-flammable dusts, liquids, wood chips and hazardous dusts with an exposure limit value of ≧ 0.1 mg/m³. The appliance must be equipped with a suitable filter corresponding to the hazard classification of the dusts to be picked up. 
Description
Product overview
 
     - Electric tool power outlet
- Automatic filter cleaning
- "Filter cleaning ON/OFF" button (only UL and UME)
- "Automatic filter cleaning system" status indicator
- Control switch
- Intake fitting
- Waste material container
- Grip recess
- Catch
- Suction head
- Grip
- Supply cord hook
- Catch for filter cover
Intended use
The products described here are industrial vacuum cleaners designed for universal, commercial use. They may be used for wet or dry applications.
Use of the product to clean down persons or animals is not permissible. Underwater use is not permissible.
- Before beginning work with the product, find out how to operate it correctly and about any hazards associated with the materials you will be working with and how these materials can be disposed of safely.
- Do not use the product for continuous, stationary operation in automatic or semi-automatic systems.
- To reduce the risk of injury, use only genuine Hilti accessories and accessory tools.
- Use an antistatic suction hose in order to avoid electrostatic effects.
- Do not pick up objects or materials that could cause injury by piercing through the dust bag (e.g. pointed or sharp objects).
- Do not stand on the product (do not use it as a substitute for a ladder).
This product is suitable for the following applications in commercial use:
- Collecting large quantities of dust from Hilti diamond grinders, diamond cutters, rotary hammers and core drilling machines using dry-cutting core bits.
- Picking up drilling slurry (mineral materials) from Hilti diamond core bits or Hilti diamond saws and liquids up to a temperature of < 60 °C (140 °F).
- Picking up oil or liquid substances with a temperature of up to < 60 °C (140 °F).
- Wet and/or dry cleaning of wall and floor surfaces.
Picking up dry, non-flammable dusts, liquids, wood chips and hazardous dusts with an exposure limit value of > 1 mg/m³ (Dust Class L).
Additionally applicable to UM and UME vacuum cleanersPicking up dry, non-flammable dusts, liquids, wood chips and hazardous dusts with an exposure limit value of ≧ 0.1 mg/m³ (Dust Class M).
Additionally applicable to UL, UM and UME vacuum cleanersWith vacuum cleaners it is necessary to make provision for an adequate rate of air exchange (L) in the room in situations where the expelled air is returned to the room. Please observe national regulations.
Possible misuse
- Do not operate the industrial vacuum cleaner when it is laid on its side.
- Do not use the industrial vacuum cleaner to pick up substances that present a risk of explosion, glowing, burning or flammable substances or aggressive dusts (e.g. magnesium or aluminum dust, etc.) (exception: wood chips or shavings).
- Do not use the industrial vacuum cleaner to pick up flammable liquids (e.g. gasoline, solvents, coolants and lubricants, etc.).
- Working with materials hazardous to the health (e.g. asbestos) is not permissible.
Items supplied
Wet/dry vacuum cleaner including filter element, suction hose complete with rotatable connector (at the vacuum cleaner end) and connector for accessories, PE VC 20/40 plastic dust bag, operating instructions.
Warning tone
UM and UME vacuum cleaners emit an audible warning tone. This warning tone is emitted when the air speed in the hose drops below 20 m/s.
In order to ensure that the warning tone is emitted correctly, the hose diameter setting must be set to the diameter of the suction hose in use.
Automatic filter cleaning
The vacuum cleaner is equipped with an automatic filter cleaning system that removes most of the dust adhering to the filter element.
The filter cleaning system can be switched off by pressing the “Automatic filter cleaning ON/OFF” button and switched back on by pressing the button again.
| Status | Meaning | 
|---|---|
| LED lights. | 
 | 
| LED doesn’t light. | 
 | 
The filter cleaning system is activated automatically each time the vacuum cleaner is switched on.
The filter element is cleaned automatically by a blast of air (a pulsating noise is heard).
Instructions for use
Accessories and how they are used| Accessories | Type of use | 
|---|---|
| PE VC 20 synthetic dust bag (203854) | Working with mineral materials, wet and dry | 
| PE VC 40 synthetic dust bag (203852) | Working with mineral materials, wet and dry | 
| VC 20 paper dust bag (203858) | Working with wood | 
| VC 40 paper dust bag (203856) | Working with wood | 
| VC 20/40 dry filter (2121386) | Dry | 
| VC 20/40 universal filter (2121387) | Universal use, wet and dry | 
| VC 20/40 performance filter (2121388) | Heavy use, wet and dry | 
| Suction hose, 27 x 3.5 m AS | Wet and dry | 
| Suction hose, 36 mm | Mainly wet, not for dust | 
| Suction hose, 36 x 5 m AS | Wet and dry | 
- Use of a plastic or paper dust bag is absolutely essential with vacuum cleaners of the UM and UME type.
Technical data
Wet / dry vacuum cleaner
| VC 20 | VC 40 | |
|---|---|---|
| Dimensions (L x W x H in mm) | 505 x 380 x 500 | 505 x 380 x 610 | 
| Weight in accordance with EPTA procedure 01 | 13.0 kg | 14.7 kg | 
| Container capacity | 21 ℓ | 36 ℓ | 
| Effective dust capacity | 23 kg | 40 kg | 
| Water capacity | 13.5 ℓ | 25 ℓ | 
| Operating temperature | −10 ℃ … 40 ℃ | −10 ℃ … 40 ℃ | 
| Automatic filter cleaning, all | 15 s | 15 s | 
| Protection class | I | I | 
| Protection class | IP X4 | IP X4 | 
| AC frequency | 50 Hz … 60 Hz | 50 Hz … 60 Hz | 
Rated voltage
| ·/· | 100 Volts [V] | 110 Volts [V] | 110 Volts [V] | 200 Volts [V] | 
| Rated power input | 1200 Watts [W] | 1100 Watts [W] | 1100 Watts [W] | 950 Watts [W] | 
| Maximum load on built-in power outlet for electric tools (if fitted) | ·/· | 1600 Watts [W] | ·/· | ·/· | 
| Power-source connection (type) | VCTF 3 x 2.0 mm2 | A07 QQF 3 / 12 AWG | H07 BQF 3G 1.5 mm2 | VCTF 3 x 2.0 mm2 | 
| ·/· | 220 - 240 Volts [V] | 220 - 240 (CH) Volts [V] | 220 - 240 (GB) Volts [V] | 220 - 240 (NZ) Volts [V] | 
| Rated power input | 1200 Watts [W] | 1200 Watts [W] | 1200 Watts [W] | 1200 Watts [W] | 
| Maximum load on built-in power outlet for electric tools (if fitted) | 2400 Watts [W] | 1100 Watts [W] | 1800 Watts [W] | 1200 Watts [W] | 
| Electric supply connection (type) | H07 RNF 3G 1.5 mm2 | H07 RNF 3G 1.5 mm2 | H07 RNF 3G 1.5 mm2 | H07 RNF 3G 1.5 mm2 | 
Maximum volumetric flow rate and maximum vacuum
| VC 20-U | VC 20-UL | VC 20-UM | VC 20-UME | ||
|---|---|---|---|---|---|
| Maximum volumetric flow rate (air) | 950 W | 68 ℓ/s | ·/· | ·/· | ·/· | 
| 1100 W | 68 ℓ/s | ·/· | ·/· | ·/· | |
| 1200 W | 74 ℓ/s | ·/· | ·/· | ·/· | |
| Maximum volumetric flow rate (air) | 1100 W | ·/· | 138 m³/h | 138 m³/h | 138 m³/h | 
| 1200 W | ·/· | 150 m³/h | 150 m³/h | 150 m³/h | |
| Maximum partial vacuum | 950 W | 235 hPa | ·/· | ·/· | ·/· | 
| 1100 W | 230 hPa | 209 hPa | 209 hPa | 209 hPa | |
| 1200 W | 253 hPa | 253 hPa | 253 hPa | 253 hPa | |
| VC 40-U | VC 40-UL | VC 40-UM | VC 40-UME | ||
|---|---|---|---|---|---|
| Maximum volumetric flow rate (air) | 950 W | 68 ℓ/s | ·/· | ·/· | ·/· | 
| 1100 W | 68 ℓ/s | ·/· | ·/· | ·/· | |
| 1200 W | 74 ℓ/s | ·/· | ·/· | ·/· | |
| Maximum volumetric flow rate (air) | 1100 W | ·/· | 138 m³/h | 138 m³/h | 138 m³/h | 
| 1200 W | ·/· | 150 m³/h | 150 m³/h | 150 m³/h | |
| Maximum partial vacuum | 950 W | 235 hPa | ·/· | ·/· | ·/· | 
| 1100 W | 230 hPa | 209 hPa | 209 hPa | 209 hPa | |
| 1200 W | 253 hPa | 253 hPa | 253 hPa | 253 hPa | |
Noise and vibration information (measured in accordance with EN 60335)
The following information applies to all VC 20 and VC 40 industrial vacuum cleaners.
| Emission sound pressure level (LpA) | 73 dB(A) | 
| Uncertainty for the sound pressure level (KpA) | 2.5 dB(A) | 
| Vibration emission value | < 2.5 m/s² | 
Use of extension cords
- Use only extension cords of a type approved for the application and with conductors of adequate cross-section. Otherwise the performance of the appliance may be affected and the cord may overheat.
- Regularly check the extension cord for damage.
- Replace damaged extension cords.
- When working outdoors, use only extension cords that are approved and correspondingly marked for this application.
| Cord | AWG 16 | AWG 14 | AWG 12 | AWG 10 | 
|---|---|---|---|---|
| Conductor cross-section | 1,31 mm² | 2,08 mm² | 3,31 mm² | 5,26 mm² | 
| Conductor cross-section | 2,58 kcmil | 4,11 kcmil | 6,53 kcmil | 10,4 kcmil | 
| Cord length | 25 m | 30 m | 50 m | 100 m | 
| Cord length | 75 ft | 100 ft | 150 ft | 250 ft | 
Before use
Operating the appliance for the first time
- Open the two catches.
- Lift the vacuum cleaner top section away from the waste material container.
- Remove the accessories and packaging from the waste material container.
- Fit the vacuum cleaner top section onto the waste material container and close the two catches.
- Check to ensure that the vacuum cleaner top section is fitted correctly and secured.
- Connect the suction hose to the appliance.
Fitting a paper dust bag for picking up wood chips
 
    - Disconnect the supply cord plug from the power outlet.
- Open the two catches.
- Lift the suction head off the waste material container.
- Fit the new paper dust bag into the adapter and insert these in the waste material container.
- Fit the vacuum cleaner top section onto the waste material container.
- Close the two catches.
- Check to ensure that the vacuum cleaner top section is fitted correctly and secured.
- Connect the suction hose to the appliance.
Fitting a plastic dust bag
 
    - Disconnect the supply cord plug from the power outlet.
- Open the two catches.
- Lift the suction head off the waste material container.
- Fit a new plastic dust bag (see instructions printed on it) in the waste material container.
- Set the suction head on the waste material container and close the two catches.
Operation
Setting the hose diameter on UM and UME vacuum cleaners
- When picking up dry, non flammable dust which has an exposure limit value, or when picking up wood chips or shavings, adjust the hose diameter setting switch to the correct diameter setting for the suction hose used.
- Set the switch to the smallest hose diameter if you are using the vacuum cleaner with a Hilti hollow drill bit system.
Operation without use of the electric tool power outlet
- Check that the switch on the appliance is in the “OFF” position off before plugging the supply cord into a power outlet.
- Plug the vacuum cleaner’s supply cord into the power outlet.
- Turn the control switch to the “ON” position.
Operation with use of the power outlet on the appliance
- Unplug the vacuum cleaner’s supply cord from the power outlet.
- Check that the maximum power drawn by the electric tool is below the maximum permissible output of the power outlet on the vacuum cleaner (please refer to the “Technical data” section of the operating instructions and information printed at the power outlet on the appliance).
- Check to ensure that the electric tool is switched off before plugging its supply cord into the power outlet.
- Plug the electric tool’s supply cord into the power outlet on the vacuum cleaner.
- Plug the vacuum cleaner’s supply cord into the power outlet.
- Turn the control switch to the “Auto” position.
- Switch on the power tool.
 
Picking up dry dust
- Check that the filter element is dry and that the correct type of dust bag is fitted.
Picking up liquids
- Check the container level monitoring system.
- If possible, use a separate filter element for wet applications.
 
- After picking up liquids, open the two catches.
- Lift the vacuum cleaner top section away from the waste material container and place it on a level surface so that the filter element can dry.
- Empty the waste material container and use a water hose to rinse it out. Use a brush to clean the electrodes and clean the filter element, after allowing it to dry, by wiping it off with your hand.
- Allow the waste material container to dry.
After use of the vacuum cleaner
- Switch off the electric tool.
- Turn the vacuum cleaner control switch to the “OFF” position.
- Unplug the vacuum cleaner’s supply cord from the power outlet.
- Coil up the supply cord and hang it on the hook.
- Empty the container and clean the appliance by wiping it with a damp cloth.
- Coil up the suction hose.
- Store the vacuum cleaner in a secure, dry place where it is inaccessible to unauthorized users.
Emptying dry dust from the waste material container
- Unplug the supply cord from power outlet.
- Lift the vacuum cleaner top section away from the waste material container and place it on a level surface.
 - Applicable to UM and UME vacuum cleaners 
 - Remove the dust bag from the waste material container.
 
- Remove the dust bag from the waste material container.
 - Applicable to U and UL vacuum cleaners 
 - Remove the dust bag from the waste material container or grip the container by the recess provided and empty it by tipping out the contents.
 
- Remove the dust bag from the waste material container or grip the container by the recess provided and empty it by tipping out the contents.
 
- Applicable to UM and UME vacuum cleaners 
- Then fit the vacuum cleaner top section onto the waste material container and close the two catches.
Emptying the waste material container when no dust bag is fitted (picking up liquids)
- Disconnect the supply cord plug from the power outlet.
- Lift the vacuum cleaner top section away from the waste material container and place it on a level surface.
- Grip the waste material container by the recess provided and empty it by tipping out the contents.
- Clean the edge of the waste material container with a cloth.
- Fit the vacuum cleaner top section onto the waste material container and close the two catches.
Care and maintenance
Care and maintenance of the appliance
- Keep the appliance, especially its grip surfaces, clean and free from oil and grease. Do not use cleaning agents containing silicone.
- Never operate the vacuum cleaner when the air vents are blocked. Clean the air vents carefully using a dry brush. Do not permit foreign objects to enter the interior of the appliance.
- Clean the outer surfaces of the appliance with a slightly damp cloth at regular intervals. Do not use a spray system, pressure jet washer or running water for cleaning as this may negatively affect the electrical safety of the appliance.
The appliance must be handled for cleaning and maintenance in a way that avoids exposing maintenance personnel and other persons to any hazards.
- Use filtered forced ventilation.
- Wear personal protective equipment.
- Clean the maintenance area in a way that prevents hazardous substances escaping into the surrounding environment.
- Vacuum off the outer surfaces of the appliance and wipe it clean or seal it in a suitable container, e.g. large plastic bag, before removing it from an area contaminated with hazardous substances. This will help to avoid distribution of the hazardous dust deposited on it.
- When maintenance or repairs are carried out, all contaminated parts which cannot be satisfactorily cleaned must be packed in impermeable bags and disposed of in compliance with the applicable disposal regulations.
- The appliance must be subjected to a technical inspection by Hilti Service or a trained person at least once a year to check, for example, for damage to the filter, air leakage, and to ensure correct operation of controlling devices.
Automatic filter cleaning
The condition of the filter element deteriorates with use.
- Replace the filter element at least every six months.
- However, if used intensively, the filter element should be replaced more often.
Changing the filter element
 
    - Disconnect the supply cord plug from the power outlet.
- Open the filter cover catches.
- Open the filter cover.
- Carefully remove the filter element, gripping it at the areas provided in the holder.
- Clean the sealing surface with a cloth.
- Fit the new filter element.
- Close the filter cover by flipping the cover catch forward.
- Close the filter cover catch.
Checking the container level monitoring system
 
    - Engage the wheel brakes so that the vacuum cleaner stands securely.
- Disconnect the supply cord plug from the power outlet.
- Open the two catches.
- Lift the vacuum cleaner top section away from the waste material container and place it on a level surface.
- Check the cut-out contacts and clean them with a brush if necessary (if dirty).
- Check the seal at the vacuum cleaner top section and clean it with a cloth if necessary.
- Fit the vacuum cleaner top section onto the waste material container and close the two catches.
Checks after cleaning and maintenance
- After cleaning or carrying out maintenance, check that the vacuum cleaner is assembled correctly and that it functions faultlessly.
- Test each of the functions.
Transport and storage
Transport
Do not carry the appliance when it is full of waste material.
The appliance may not be lifted directly by crane.
- Remove the power conditioner (if applicable) or loose accessory tools from the holder.
- Empty the appliance before carrying it to another location.
- Do not tip the appliance or transport it lying on its side after using it to pick up liquids.
- Use the tapered adapter to connect both ends of the hose together conveniently for transport.
Storage
- Store the vacuum cleaner in a secure, dry place where it is inaccessible to unauthorized users.
Troubleshooting
If the trouble you are experiencing is not listed in this table or you are unable to remedy the problem by yourself, please contact Hilti Service.
Troubleshooting table
| Malfunction | Possible cause | Action to be taken | 
|---|---|---|
| UM and UME vacuum cleaners: Acoustic warning signal (reduced suction power) | The dust bag is full. | 
 | 
| The filter element is clogged with dirt or dust. | 
 | |
| The suction hose or dust hood on the electric tool is blocked. | 
 | |
| The hose diameter setting is incorrect. | 
 | |
| Dust is blown out of the appliance. | The filter element is not fitted correctly. | 
 | 
| The filter element is damaged. | 
 | |
| The appliance switches itself off or on inadvertently or static electricity discharges through the user. | Electrostatic charge is not conducted away – the appliance is connected to an unearthed/ungrounded power outlet. | 
 | 
| The appliance doesn’t start or switches itself off after a short time. | The water level cut-out is activated. | 
 | 
| The motor doesn’t restart. | The mains circuit breaker has been tripped. | 
 | 
| The waste material container is full. | 
 | |
| The motor overheating protection cut-out has been activated. | 
 | |
| The motor is repeatedly switched off by its thermal cut-out. | 
 | |
| The motor doesn’t run when set to “AUTO”. | The appliance is faulty or is not correctly plugged in. | 
 | 
| The automatic filter element cleaning system doesn’t work. | No suction hose is connected. | 
 | 
Disposal
 Most of the materials from which Hilti products are manufactured can be recycled. The materials must be correctly separated before they can be recycled. In many countries, your old tools, machines or appliances can be returned to Hilti for recycling. Ask Hilti Service or your Hilti representative for further information.
 Most of the materials from which Hilti products are manufactured can be recycled. The materials must be correctly separated before they can be recycled. In many countries, your old tools, machines or appliances can be returned to Hilti for recycling. Ask Hilti Service or your Hilti representative for further information.
In accordance with the European Directive on waste electrical and electronic equipment and its implementation in conformance with national law, electric tools or appliances that have reached the end of their life must be collected separately and returned to an environmentally compatible recycling facility.
Drilling slurryDisposal of drilling slurry directly into rivers, lakes or the sewerage system without suitable pretreatment presents environmental problems.
- Ask the local public authorities for information about current regulations.
We recommend the following pretreatment:
- Collect the drilling slurry (for example, using a wet-type vacuum cleaner).
- Allow the drilling slurry to settle and dispose of the solid material at a construction waste disposal site (addition of a flocculent may accelerate the settling process).
- The remaining water (alkaline, pH value greater than 7) must be neutralized by the addition of an acidic neutralizing agent or diluted with a large volume of water before it is allowed to flow into the sewerage system.
- Dispose of the drilling dust collected by the vacuum cleaner in accordance with the applicable national regulations.
Manufacturer’s warranty
- Please contact your local Hilti representative if you have questions about the warranty conditions.