HDE 500‑A12
 Original operating instructions
Information about the documentation
About this documentation
- Read this documentation before initial operation or use. This is a prerequisite for safe, trouble-free handling and use of the product.
- Observe the safety instructions and warnings in this documentation and on the product.
- Always keep the operating instructions with the product and make sure that the operating instructions are with the product when it is given to other persons.
Explanation of symbols
Warnings
Warnings alert persons to hazards that occur when handling or using the product. The following signal words are used:Symbols in the operating instructions
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
The following symbols are used in illustrations:|  | These numbers refer to the illustrations at the beginning of these operating instructions. | 
|  | The numbering reflects the sequence of operations shown in the illustrations and may deviate from the steps described in the text. | 
|  | Item reference numbers are used in the overview illustration and refer to the numbers used in the key in the product overview section. | 
|  | These characters are intended to specifically draw your attention to certain points when handling the product. | 
Product-dependent symbols
Symbols on the product
The following symbols can be used on the product:|  | National waste-materials management system | 
|  | “Off” position | 
|  | Continuous dispensing | 
|  | Measured dispensing 5...80 ml | 
|  | Measured dispensing 1...16 | 
|  | Direct current (DC) | 
|  | The product supports near-field communication (NFC) technology compatible with iOS and Android platforms. | 
|  | Li-ion battery | 
|  | Never use the battery as a striking tool. | 
|  | Do not drop the battery. Never use a battery that has suffered an impact or is damaged in any other way. | 
|  | Hilti Li-ion battery type series used. Observe the information given in the section headed Intended use . | 
|  | If applied on the product, the product has been certified by this certification body for the US and Canadian markets according to the applicable standards. | 
Product information
 products are designed for professional users and only trained, authorized personnel are permitted to operate, service and maintain the products. This personnel must be specifically informed about the possible hazards. The product and its ancillary equipment can present hazards if used incorrectly by untrained personnel or if used not in accordance with the intended use.
 products are designed for professional users and only trained, authorized personnel are permitted to operate, service and maintain the products. This personnel must be specifically informed about the possible hazards. The product and its ancillary equipment can present hazards if used incorrectly by untrained personnel or if used not in accordance with the intended use.
   The type designation and serial number are printed on the rating plate.
- Write down the serial number in the table below. You will be required to state the product details when contacting Hilti Service or your local Hilti organization to inquire about the product.
 Product informationCordless dispenser: HDE 500-A12 Generation: 01 Serial number: 
Safety
General power tool safety warnings
 WARNING 
   Read all safety warnings, instructions, illustrations and specifications provided with this power tool. Failure to follow all instructions listed below may result in electric shock, fire and/or serious injury.
 
   WARNING 
   Read all safety warnings, instructions, illustrations and specifications provided with this power tool. Failure to follow all instructions listed below may result in electric shock, fire and/or serious injury.
   Save all warnings and instructions for future reference.
The term "power tool" in the warnings refers to your mains-operated (corded) power tool or battery-operated (cordless) power tool.
Work area safety
- Keep work area clean and well lit. Cluttered or dark areas invite accidents.
- Do not operate power tools in explosive atmospheres, such as in the presence of flammable liquids, gases or dust. Power tools create sparks which may ignite the dust or fumes.
- Keep children and bystanders away while operating a power tool. Distractions can cause you to lose control.
- Power tool plugs must match the outlet. Never modify the plug in any way. Do not use any adapter plugs with earthed (grounded) power tools. Unmodified plugs and matching outlets will reduce risk of electric shock.
- Avoid body contact with earthed or grounded surfaces, such as pipes, radiators, ranges and refrigerators. There is an increased risk of electric shock if your body is earthed or grounded.
- Do not expose power tools to rain or wet conditions. Water entering a power tool will increase the risk of electric shock.
- Do not abuse the cord. Never use the cord for carrying, pulling or unplugging the power tool. Keep cord away from heat, oil, sharp edges or moving parts. Damaged or entangled cords increase the risk of electric shock.
- When operating a power tool outdoors, use an extension cord suitable for outdoor use. Use of a cord suitable for outdoor use reduces the risk of electric shock.
- If operating a power tool in a damp location is unavoidable, use a residual current device (RCD) protected supply. Use of an RCD reduces the risk of electric shock.
- Stay alert, watch what you are doing and use common sense when operating a power tool. Do not use a power tool while you are tired or under the influence of drugs, alcohol or medication. A moment of inattention while operating power tools may result in serious personal injury.
- Use personal protective equipment. Always wear eye protection. Protective equipment such as a dust mask, non-skid safety shoes, hard hat or hearing protection used for appropriate conditions will reduce personal injuries.
- Prevent unintentional starting. Ensure the switch is in the off-position before connecting to power source and/or battery pack, picking up or carrying the tool. Carrying power tools with your finger on the switch or energising power tools that have the switch on invites accidents.
- Remove any adjusting key or wrench before turning the power tool on. A wrench or a key left attached to a rotating part of the power tool may result in personal injury.
- Do not overreach. Keep proper footing and balance at all times. This enables better control of the power tool in unexpected situations.
- Dress properly. Do not wear loose clothing or jewellery. Keep your hair and clothing away from moving parts. Loose clothes, jewellery or long hair can be caught in moving parts.
- If devices are provided for the connection of dust extraction and collection facilities, ensure these are connected and properly used. Use of dust collection can reduce dust-related hazards.
- Do not let familiarity gained from frequent use of tools allow you to become complacent and ignore tool safety principles. A careless action can cause severe injury within a fraction of a second.
- Do not force the power tool. Use the correct power tool for your application. The correct power tool will do the job better and safer at the rate for which it was designed.
- Do not use the power tool if the switch does not turn it on and off. Any power tool that cannot be controlled with the switch is dangerous and must be repaired.
- Disconnect the plug from the power source and/or remove the battery pack, if detachable, from the power tool before making any adjustments, changing accessories, or storing power tools. Such preventive safety measures reduce the risk of starting the power tool accidentally.
- Store idle power tools out of the reach of children and do not allow persons unfamiliar with the power tool or these instructions to operate the power tool. Power tools are dangerous in the hands of untrained users.
- Maintain power tools and accessories. Check for misalignment or binding of moving parts, breakage of parts and any other condition that may affect the power tool’s operation. If damaged, have the power tool repaired before use. Many accidents are caused by poorly maintained power tools.
- Keep cutting tools sharp and clean. Properly maintained cutting tools with sharp cutting edges are less likely to bind and are easier to control.
- Use the power tool, accessories and tool bits etc. in accordance with these instructions, taking into account the working conditions and the work to be performed. Use of the power tool for operations different from those intended could result in a hazardous situation.
- Keep handles and grasping surfaces dry, clean and free from oil and grease. Slippery handles and grasping surfaces do not allow for safe handling and control of the tool in unexpected situations.
- Recharge only with the charger specified by the manufacturer. A charger that is suitable for one type of battery pack may create a risk of fire when used with another battery pack.
- Use power tools only with specifically designated battery packs. Use of any other battery packs may create a risk of injury and fire.
- When battery pack is not in use, keep it away from other metal objects, like paper clips, coins, keys, nails, screws or other small metal objects, that can make a connection from one terminal to another. Shorting the battery terminals together may cause burns or a fire.
- Under abusive conditions, liquid may be ejected from the battery; avoid contact. If contact accidentally occurs, flush with water. If liquid contacts eyes, additionally seek medical help. Liquid ejected from the battery may cause irritation or burns.
- Do not use a battery pack or tool that is damaged or modified. Damaged or modified batteries may exhibit unpredictable behaviour resulting in fire, explosion or risk of injury.
- Do not expose a battery pack or tool to fire or excessive temperature. Exposure to fire or temperature above 130° C (265 °F) may cause explosion.
- Follow all charging instructions and do not charge the battery pack or tool outside the temperature range specified in the instructions. Charging improperly or at temperatures outside the specified range may damage the battery and increase the risk of fire.
- Have your power tool serviced by a qualified repair person using only identical replacement parts. This will ensure that the safety of the power tool is maintained.
- Never service damaged battery packs. Service of battery packs should only be performed by the manufacturer or authorized service providers.
Additional safety instructions
Personal safety- Never tamper with or modify the product or accessories in any way.
- Use the product and accessories only when they are in perfect working order.
- Risk of injury by falling tools and/or accessories. Before starting work, check that the battery and installed accessories are secure.
- Wear eye protection and protective gloves when changing accessories.
- Prior to use, read and comply with the safety data sheet for the product, the instructions on the packaging and the instructions for use of the foil pack.
- Begin injecting the compound until it is in the immediate working area.
- Never point the product toward yourself or other persons.
- Never leave the product unattended.
- Do not use the product if parts are damaged or if operating controls do not function faultlessly. Have the product repaired by Hilti Service.
- Keep the workplace tidy. Objects which could cause injury should be removed from the working area.
- Wear non-skid shoes.
- Take the influences of the surrounding area into account. Do not use the product where there is a risk of fire or explosion.
- Do not use faulty/worn-out foil pack holders.
Battery use and care
- Comply with the following safety instructions for the safe handling and use of Li-ion batteries. Failure to comply can lead to skin irritation, severe corrosive injury, chemical burns, fire and/or explosion.
- Use only batteries that are in perfect working order.
- Treat batteries with care in order to avoid damage and prevent leakage of fluids that are extremely harmful to health!
- Do not under any circumstances modify or tamper with batteries!
- Do not disassemble, crush or incinerate batteries and do not subject them to temperatures over 80 °C (176 °F).
- Never use or charge a battery that has suffered an impact or been damaged in any other way. Check your batteries regularly for signs of damage.
- Never use recycled or repaired batteries.
- Never use the battery or a battery-operated power tool as a striking tool.
- Never expose batteries to the direct rays of the sun, elevated temperature, sparking, or open flame. This can lead to explosions.
- Do not touch the battery poles with your fingers, tools, jewelry, or other electrically conductive objects. This can damage the battery and also cause material damage and personal injury.
- Keep batteries away from rain, moisture and liquids. Penetrating moisture can cause short circuits, electric shock, burns, fire and explosions.
- Use only chargers and power tools approved for the specific battery type. Read and follow the relevant operating instructions.
- Do not use or store the battery in explosive environments.
- If the battery is too hot to touch, it may be defective. Put the battery in a place where it is clearly visible and where there is no risk of fire, at an adequate distance from flammable materials. Allow the battery to cool down. If it is still too hot to touch after an hour, the battery is faulty. Consult Hilti Service or read the document entitled "Instructions on safety and use for Hilti Li-ion batteries".
 
Description
Overview
 
     - Front locating lug for installation of the foil pack holder / cartridge
- Cradle for the foil pack holder / cartridge
- Rear locating lug for installation of the foil pack holder / cartridge
- Dispensing mode selector switch
- Parallel piston rods with grip
- Release button
- Grip
- Battery
- Battery release buttons (also used to activate the charge status indicator)
- Trigger
- Foil pack
- Foil pack holder, black
- Foil pack holder, red
- Cartridge
Intended use
The product is designed to dispense the contents of Hilti foil packs and cartridges in a controlled operation. The HDE 500‑A12 cordless dispenser is designed exclusively for use with Hilti 330 ml or 500 ml foil packs and 580 ml cartridges.
The product can be used with either a foil pack holder or a cartridge: 
    - Use only Hilti Li-ion batteries of the B12 series with this product. For optimum performance, Hilti recommends the batteries stated in the table at the end of these operating instructions for this product. 
- For these batteries, use only Hilti chargers of the type series stated in the table at the end of these operating instructions. 
Items supplied
Dispenser and operating instructionsOther system products approved for use with this product can be found at your local Hilti Store or at: www.hilti.group
Charge state display
The charge state of the Li‑ion battery is displayed after pressing one of the release buttons lightly (press only until slight resistance is felt).| Status | Meaning | 
|---|---|
| 4 LEDs show. | Charge state: 75 % to 100 % | 
| 3 LEDs show. | Charge state: 50 % to 75 % | 
| 2 LEDs show. | Charge state: 25 % to 50 % | 
| 1 LED shows. | Charge state: 10 % to 25 % | 
| 1 LED flashes. | 
 | 
Technical data
| HDE 500-A12 | |
|---|---|
| Weight without battery | 1.8 kg (4.0 lb) | 
| Rated voltage | 10.8 V | 
| Storage temperature | −40 ℃ …85 ℃ (−40 ℉ …185 ℉) | 
| Ambient temperature for operation | −17 ℃ …60 ℃ (1 ℉ …140 ℉) | 
Battery
| Battery operating voltage | 10.8 V | 
| Weight, battery | See the end of these operating instructions | 
| Ambient temperature for operation | −17 ℃ …60 ℃ (1 ℉ …140 ℉) | 
| Storage temperature | −40 ℃ …85 ℃ (−40 ℉ …185 ℉) | 
| Battery charging starting temperature | −10 ℃ …45 ℃ (14 ℉ …113 ℉) | 
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
- Press the battery release buttons.
- Remove the battery from the product.
Fall arrest
As drop arrester for this product, use the Hilti tool tether #2261970 or #2261971.- Secure the carabiner to a load-bearing structure. Check that the carabiner holds securely.
- Depending on which type of Hilti tool tether is used, secure either the second carabiner or the loop to the product as shown in the illustration. Check that it holds securely.
 
 
     Inserting the foil pack holder and foil pack
 
    - Press the release button.
- Pull the piston rod back as far as they will go.
- Fit the front end of the foil pack holder into the front locating lug.
- Pull the foil pack holder on to the rear locating lug and swivel the foil pack holder up.
- Screw the static mixer (mixing nozzle) onto the foil pack.
- Push the foil pack into the foil pack holder.
- Swivel the foil pack holder into the dispenser.
Inserting the cartridge
 
    - Press the release button.
- Pull the piston rod back as far as they will go.
- Fit the front end of the cartridge into the front locating lug.
- Pull the cartridge on to the rear locating lug and swivel the cartridge up.
- Screw the static mixer (mixing nozzle) onto the foil pack.
- Swivel the cartridge into the dispenser.
Manually discarding the initial quantity of mortar
 
    - Set the dispensing mode selector switch to  . .
- Squeeze the trigger until the mixing nozzle is completely full.
- Set the dispensing mode selector switch to the appropriate volume of mortar for discarding  . .
 
- Discard the initially dispensed volume of mortar.
Operation
Observe the safety instructions and warnings in this documentation and on the product.Injecting mortar
 
    - Press the trigger.
- Inject the mortar.
Removing the foil pack holder and foil pack
 
    - Set the dispensing mode selector switch to  . .
- Press the release button.
- Pull the piston rod back as far as they will go.
- Swivel the foil pack holder up.
- Remove the foil pack.
- Press the tab on the foil pack holder.
- Press the foil pack holder down at the rear locating lug.
- Pull the foil pack holder down from the front locating lug.
Removing the cartridge
 
    - Set the dispensing mode selector switch to  . .
- Press the release button.
- Pull the piston rod back as far as they will go.
- Swivel the cartridge upwards.
- Press the cartridge down at the rear locating lug.
- Pull the cartridge down from the front locating lug.
Care and maintenance
Care of the product- Carefully remove stubborn dirt.
- Carefully clean the ventilation slots, if present, with a dry brush.
- Use only a slightly damp cloth to clean the casing. Do not use cleaning agents containing silicone as these can attack the plastic parts.
- Oil the piston rods when necessary.
- Never use a battery with clogged ventilation slots. Clean the ventilation slots carefully using a dry, soft brush.
- Avoid unnecessary exposure of the battery to dust and dirt. Never expose the battery to high levels of moisture (e.g. by being dipped in water or left in the rain).
 If a battery has been soaked by moisture, treat it as a damaged battery. Isolate it in a non-flammable container and consult Hilti Service.
- Keep the battery free of oil and grease. Do not permit dust or dirt to accumulate unnecessarily on the battery. Clean the battery with a dry, soft brush or a clean, dry rag.
 Do not use cleaning agents containing silicone as these can attack the plastic parts.
- Use only a slightly damp cloth to clean the casing. Do not use cleaning agents containing silicone as these can attack the plastic parts.
- Check all visible parts and controls for signs of damage at regular intervals and make sure that they all function correctly.
- Do not operate the product if signs of damage are found or if parts malfunction. Have it repaired immediately by Hilti Service.
- After cleaning and maintenance, fit all guards or protective devices and check that they function correctly.
Transport and storage of cordless tools and batteries
Transport- Remove the battery/batteries.
- Never transport batteries loose and unprotected. During transport, batteries should be protected from excessive shock and vibration and isolated from any conductive materials or other batteries that may come in contact with the terminals and cause a short circuit. Comply with the locally applicable regulations for transporting batteries. 
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
Transport and storage of dispensers
- For transporting and storing the tool, set the dispensing mode selector switch to  . .
Troubleshooting
If the trouble you are experiencing is not listed in this table or you are unable to remedy the problem by yourself, please contact Hilti Service.Troubleshooting
If a problem occurs, always observe the charge-status and fault indicator of the battery. See the section headed Status indicators of the Li‑ion battery .If the trouble you are experiencing is not listed in this table or you are unable to rectify the problem by yourself, contact Hilti Service.
| Trouble or fault | Possible cause | Action to be taken | 
|---|---|---|
| Product does not work. | The battery is not fully inserted. | 
 | 
| Battery is discharged. | 
 | |
| Dispensing mode selector switch set to  | 
 | |
| The battery does not engage with an audible click. | The retaining lug on the battery is dirty. | 
 | 
| The product or battery gets very hot. | The product is overloaded (application limits exceeded). | 
 | 
| Electrical fault | 
 | |
| The battery runs down more quickly than usual. | Very low ambient temperature. | 
 | 
| Product prematurely aborts dispensing operation | The overload cut-out is activated; mortar in the mixing nozzle has hardened | 
 | 
| The overload cut-out is activated; The dispensing pressure required is too high for the product. | 
 | |
| Foil pack empty | 
 | |
| The foil pack holder cannot be swiveled into the product. | The foil pack is not pushed fully into the holder. | 
 | 
| Piston rods not pulled back fully | 
 | |
| The foil pack holder does not engage with an audible click | The retaining lugs are dirty | 
 | 
| The retaining lugs are defective | 
 | |
| No mortar is dispensed from the mixing nozzle | Mortar in the mixing nozzle has hardened | 
 | 
Disposal
 Most of the materials from which 
  Hilti products are manufactured can be recycled. The materials must be correctly separated before they can be recycled. In many countries, your old tools, machines or appliances can be returned to 
  Hilti for recycling. Ask 
  Hilti Service or your Hilti sales representative for further information.
 Most of the materials from which 
  Hilti products are manufactured can be recycled. The materials must be correctly separated before they can be recycled. In many countries, your old tools, machines or appliances can be returned to 
  Hilti for recycling. Ask 
  Hilti Service or your Hilti sales representative for further information.
  Manufacturer’s warranty
- Please contact your local Hilti representative if you have questions about the warranty conditions.
Further information
 
   This link is also to be found at the end of the documentation, in the form of a QR code.